FAQs Techniques

Poser une question

Filtre de Résultat

    What are the basic troubleshooting steps for the APC Back-UPS Pro with Networking bg500 ?
    The Back-UPS battery is completely discharged. Connect the Back-UPS to AC power and allow the battery to recharge for 12 hours.
    Battery Damage When Battery Is Left Discharged
    When a battery is allowed to ... Allowing batteries to stand for ... ... sulfate on the battery plates. ... inability of the battery to retain charge ... A charged battery , disconnected from ... A discharged battery needs to be ... to avoid permanent battery damage. ... UPS with the battery connected can cause permanent battery damage within a ... ... stored after complete battery recharging with the battery disconnected. ... (VRLA) batteries should be immediately ... VRLA batteries should recover fully ... No VRLA battery should ever be ... VDC for a 12 volt battery ). ... replace the affected batteries .
    Unattended Graceful Shutdown of Cisco Unity Express with an APC UPS
    An APC Smart-UPS ... combination with the APC ap9840 shutdown serial ... ... IOS Software Release 12 .3( ... work with the APC Smart-UPS ... ... signal form the APC UPS, the ... ... is compatible with APC’s Smart-UPS ... The Smart-UPS will only initiate the shutdown command after its battery capacity has reached less than 5 percent. ... After the loss of AC power, the APC UPS requires the shutdown signal to be asserted for at least 4 seconds before the APC UPS shuts down. ... If this happens, the APC UPS will not shut down the router at all.
    Why is my actual UPS runtime different from the quoted runtime on the APC web page?
    ... runtime on the APC web page? ... runtime on the APC web page? ... temperature of the battery within its environment ... ... Age of the battery ... - A new battery will only reach ... Temperature & battery life ... capacity of a battery will increase at ... Recharging the battery ... - Whilst a battery will recharge to ... ... because as the battery approaches its fully ... back into the battery . ... capacity of the battery , reducing with ... ... - When a battery is stored, ... ... exceeded the typical battery manufactures specification the battery will return to ... Typical maximum storage period is 12 months at 25 deg ...
    Video: How to verify USB device drivers are loaded in Windows OS
    The USB drivers for communications between APC UPS and Windows OS are pre-installed in the Windows OS. The drivers should load automatically once the APC UPS has been connected to the computer using the proper USB cable. ... Microsoft Windows Vista, 7, 8x, 10, Server 10, 12 ,16 ... To view the drivers go to Control Panel -> Device Manager -> Batteries . There you should see either HID UPS Battery or APC UPS.
    What are the basic troubleshooting steps for the Back-UPS Connect model bg500?
    APC Back-UPS ... The battery is not connected ... Connect the battery . ... "Connect the Battery " on page ... ... power and the battery is connected, ... ... cold boot when battery capacity is less ... The battery does not charge ... the outlets The battery will not charge ... ... ON/Replace Battery LED flashes and ... constant tone The battery is disconnected. ... "Connect the Battery " section of ... ... Back-UPS battery is completely discharged ... ... and allow the battery to recharge for 12 hours. Contact APC Technical Support for ... ... is operating on battery power.
    Stacking limitations for single phase Symmetra and Matrix products
    Although instructions are provided for these stacking options, APC always recommends the use of its field service group to complete these procedures. ... APC offers Symmetra LX Tower systems with integrated XR battery cabinets (ex. ... The UPS and batteries can be stacked up to 62" high. ... Do NOT stack anything on top or below a SYXR12 12 - Battery XR Cabinet or SYMSTRF 16kva UPS Systems. ... The UPS and batteries can be stacked 36.6"" high.
    acdc1010 Hot Aisle Containment Rack Expansion Bundle Kit Installation (Manual)
    ... , or XR Battery Cabinet is receiving ... ... , or XR Battery Cabinet, in ... ... , or XR Battery Cabinet. ... M6× 12 mm screws and ... available from APC . Attach the ... ... , or XR Battery Cabinet Use six M6 × 12 -mm ... Use an M6 × 12 -mm screw and a flange nut for each bracket. ... Use five M6 × 12 -mm screws and M6 flange nuts on each upright. ... APC offers an optional grounding kit (ar8390) for grounding an enclosure. ... APC offers an optional grounding kit (ar8390) for grounding an enclosure
    How do I recycle APC batteries in the US and Canada?
    Issue: How do I recycle APC batteries in the US and Canada?
    What is the expected life of my APC UPS battery?
    Most APC batteries should last three to five years. There are many factors which affect Battery life including environment and number of discharges.
    Résultats 1 - 10 de 92