Consulter la FAQ



Where can I get support for APC and MGE Products?
-5 3888YL- 50 3888YL-7 3888YL-75 3984- ... 3984-BL 3984-GR 3984- WH 40028-8 ...
Configuring Microsoft Vista, Windows 7, 8, & 10, Windows 2008 & 2012 to safely shutdown without using APC's PowerChute software.
Once a USB UPS is connected, the OS adds configuration similar to that of a laptop with an on-board battery .
Why is my actual UPS runtime different from the quoted runtime on the APC web page?
- Whilst the capacity of a battery will increase at higher temperatures its life will be reduced, typically by 50 % for every 10 ...
Video: How do I adjust Battery Test settings ​on my Symmetra PX 250-500 UPS
... How to adjust Battery Test settings The battery self-test ... health of the battery modules in your ... ... to detect failing batteries and to ensure ... Battery self-test ... ... when choosing your battery self-test ... ... runtime available as batteries age. ... drain on the batteries . ... UPS load, battery age is also ... Enter the user password ( apc by default) Press ‘ Battery Test Settings’ ... Your battery charge must be at least 50 % for a battery self test, 100% for a runtime calibration. ... Tap Start to begin the battery runtime calibration or self test.
What are the basic troubleshooting steps for the APC Back-UPS Pro with Networking bg500 ?
APC APC ... find the your APC AV J- ... battery capacity The battery is not connected ... Connect the battery . ... "Connect the Battery " section of ... ... power and the battery is connected, ... ... On/Replace Battery LED flashes and ... The battery is disconnected. ... "Connect the Battery " section of ... The battery is completely discharged ... ... and allow the battery to recharge for ... Contact APC Technical Support for ... ... is operating on battery power. ... operating normally on battery power. ... is restored the battery will recharge. The battery has approximately two ... The battery is near a ...
How do I recycle APC batteries in the US and Canada?
Issue: How do I recycle APC batteries in the US and Canada?
What is the expected life of my APC UPS battery?
Most APC batteries should last three to five years. There are many factors which affect Battery life including environment and number of discharges.
Why should I use only genuine APC Replacement Battery Cartridge (RBC) in my APC UPS?
Using of a non- APC battery may result in lower runtime, damage the UPS, create hazardous conditions, or void safety certifications ...
Why aren't alarms clearing in the BMS (Battery Management System) AP9921X-AP9922 after replacing batteries?
After changing a battery in a string which is monitored by the APC Battery Management System, it is imperative to clear the old baseline ...
Complying with U.S. Department of Transportation (DOT) Shipping Regulations for Sealed Lead-Acid Batteries
All the batteries APC ships meet the requirements of UN Number 2800 ("" Batteries , wet, non-spillable"") ...


Résultats 1 - 10 de 92

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.