FAQs Techniques

Poser une question

Filtre de Résultat

    Are there any NetShelter products or solutions certified by Cisco?
    NetShelter SX Accessories ... -Rack Power Distribution with Cisco Energywise ... Being Cisco Certified isn't the " end all be all" for solutions.
    How do you install an Isolated Extension Cable with a Share-UPS?
    Accessory Guidelines If you want to ensure UPS ON capability, connect the accessory to the UPS end .
    InfraStruXure Automatic Transfer Switch with Power Distribution (ATS); Operation manual, how to operate
    This manual is intended for end -users of the InfraStruXure Automatic Transfer Switch with Power Distribution (ATS).
    APC UPS Network Management Card (NMC) Compatibility Chart
    This add-on option is only able to monitor the UPS, and not any power distribution .
    Is COO, HTTS or ECCN information available for NetShelter CX cabinets and accessories?
    ar4038i NetShelter CX 38U 750 mm Wide x 1130 mm Deep Enclosure Oak/Grey Finish Intl
    Where can I get support for APC and MGE Products?
    Air Distribution Accessories ... AIS Accessories ... AV Accessories ... Back-UPS Accessories ... Cabinet Power Distribution ... Configurable Power Accessories Configurable Power Distribution ... Data Distribution Cable ... DC Distribution Components ... Hardwire Surge Suppression Accessories ... Matrix-UPS Accessories ... MGE Accessories ... Modular Power Accessories Modular Power Distribution ... NetBotz Accessories and Cables ... NetShelter Open Frame Rack Accessories ... NetworkAIR Accessories ... Power Distribution Units ... Rack PDU Accessories ... Refrigerant Distribution ... Room Cooling Accessories ... Row Cooling Accessories ... Silcon Accessories ... Smart-UPS Accessories ... Stationary Power Distribution Units ... Symmetra Accessories ... Symmetra MW Accessories ... Symmetra PX Accessories ... TSP Accessories ... Universal Power Accessories
    ITI (CBEMA) Curve
    This region describes a decaying ringwave transient which typically results from the connection of power-factor-correction capacitors to an AC distribution system. The frequency of this transient may range from 200hz to 5khz, depending upon the resonant frequency of the AC distribution system. ... The transient is assumed to be completely decayed by the end of the half-cycle in which it occurs.
    InRow RC Standard and Optional Features
    2-Other Optional Features or accessories are as follow: ... Power Trough (Overhead power distribution between racks)
    Résultats 1 - 10 de 92