Consulter la FAQ



Verification of Matrix-UPS input voltage configuration
The North American Matrix- UPS 3000 and 5000 units are wired at the factory for a 208 Vac input.
No power output from the Matrix-UPS L14-30 or 5-15 receptacles (mx3000/5000)
This breaker controls the UPS output to the L14-30 receptacle ... -15 receptacles on the Matrix- UPS 3000 model only).
UPS Signalling Bundle for IBM AS/400 & IBMi (IBM Power Systems)
The cable connector end labeled " UPS " is connected to the UPS (or the 940- 3000 dongle if required).
MGE STS, Galaxy 3000, 4000, 5000 and Galaxy PW; Wiring information for egx100 to any 66061-supported products
This assumes only one 66061 card or UPS or STS is connected to the enclosure but if more than one change as required.
Where can I get support for APC and MGE Products?
AIS 3000 ... Basic Rack PDU ... Charge- UPS EX ... Magnum VS ... Matrix- UPS Matrix- UPS Accessories Metered Rack PDU Metered-by-Outlet Rack PDU ... MGE Galaxy 3000
Network Management Card 660674/34003640se; ripple20 vulnerability status
... STS, Upsilon STS, eps6000, eps7000, eps8000, Galaxy 4000, Galaxy 3000 , Galaxy PW, Comet, MGE, 660674 ...


Résultats 1 - 10 de 63

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.