Sfoglia le FAQ

Video: Connect Battery on Back-UPS RS/NS M2 & MS Series

Data di pubblicazione: 10 October 2019

Issue:
Tutorial for connecting or replacing the internal battery on Back-UPS Pro RS/NS M2 & MS series. The UPS will indicate a disconnected battery by flashing an empty battery icon on its front display.

Product Line:
Back-UPS Pro RS/NS

Environment: 
BR1000MS/BR1350MS/BR1500MS
BN1100M2/BN1350M2/BN1375M2/BN1500M2

Cause:
All APC UPS systems are shipped with batteries disconnected to comply with US DOT regulations. The UPS will flash the battery icon to indicate a disconnected battery state.
A severely discharged/damaged battery will also generate the flashing battery alert. The Back-UPS will not be able to recharge or otherwise use a severely discharged battery.

Resolution: 
To connect, disconnect or replace the internal battery, please follow the steps indicated in the video and images below.




E' stato utile?

Che cosa possiamo fare per migliorare l'informazione?

Non trovi quello che cerchi?

Contatta l'assistenza clienti per ricevere informazioni, supporto tecnico, assistenza per i reclami e altro ancora.