Sfoglia le FAQ



Data Center Expert | How do hardware and software support contracts work?
... hardware warranty and software support contracts work for StruxureWare Data Center Expert. StruxureWare Data Center Expert (DCE ... StruxureWare Data Center Expert (all ... Software Support Contract StruxureWare Data Center Expert appliances come ... software support. The Data Center Expert appliance and ... active and complete software support in order ... technical support and software upgrades. Software support contracts are required for the server which has a default 25 nodes (covered under base software support SKUs) ... as each additional node license. StruxureWare Data Center Expert Appliances can ... Year 1 Software Support Contracts Software support can not ...
Data Center Expert | Why does StruxureWare not accept my One Time passcode?
StruxureWare Data Center Expert is not ... StruxureWare Data Center Expert (DCE ... StruxureWare Data Center Expert (all ... SturuxureWare Data Center Expert requires a ... and the Data Center Expert's MAC address ... StruxureWare Data Center Expert (DCE ... ... this, the server registers itself in ... ... notifies the DCE server that there is ... ... Afterwards, the server scans the unit ... 1 . In a ... ... add a new server , please click ... ... against an existing server please jump to ... ... = StruxureWare Data Center Expert Basic ... = StruxureWare Data Center Expert Standard ... = StruxureWare Data Center Expert Enterprise
Data Center Expert | What virtualization environments are supported?
... for the Data Center Expert virtual appliance ... StruxureWare Data Center Expert (DCE ... StruxureWare Data Center Expert (all ... ... EcoStruxure IT Help Center at: ... -Data- Center -Expert- ... The Data Center Expert v7.x server is available as ... ... to five device nodes and one surveillance node . ... monitor additional device nodes and activate supported applications , or to migrate from a server hardware version to ... ... of the Data Center Expert 7. ... The Data Center Expert virtual appliance is delivered as an OVA (Open Virtualization Archive), expected to function properly on ...
Assigning global permission for newly created user is not allowed in vSphere vCenter 6.0 U 1b and 6.0 U 2a.
vCenter cluster having more than two nodes . vCenter Server is installed on ... ... your windows vCenter Server ... c:\ Program Files\MIT ... Copy the path (eg: c:\ Program Files\MIT\Kerberos\bin) Navigate to the registry path: HKEY_USERS\S- 1 -5-18\Environment ... eg: C:\ Program Files\*******; c:\ Program Files\MIT\Kerberos\bin ... Restart the Windows vCenter server
Data Center Expert | Migrating from a Physical Appliance to a Virtual Appliance
... base . Note that if your previous server already has licensing on it (beyond the base 25 device nodes and 1 surveillance node ) ...
Data Center Expert | How do I upgrade my software version?
Process for upgrading StruxureWare Data Center Expert. ... StruxureWare Data Center Expert (DCE) - Basic Appliance (AP9465) ... StruxureWare Data Center Expert (all versions) ... You must have a valid currently active software support contract to receive upgrade files. ... 1 ) Download the upgrade.zip ... 3) Login to the DCE Desktop Client, select the Updates Menu, and then select Apply Server Update. ... 5) Select Install Update to start upgrading the server .
Data Center Expert | Getting Started
... with a Data Center Expert Appliance. StruxureWare Data Center Expert (DCE ... StruxureWare Data Center Expert (all ... ... the Physical Data Center Expert Appliance ... the Virtual Data Center Expert Appliance ... restricted to 5 nodes . ... the StruxureWare Data Center Expert Virtual Appliance ... ... storage that Data Center Expert has within ... Getting Data Center Expert on the ... ... that your Data Center Expert (DCE ... ... for StruxureWare Data Center Expert StruxureWare Data Center Expert Security Information ... Licensing and Software Support Data Center Expert requires continuous software support to receive ... How do software support contracts work ...
Video: Data Center Operation | Copying files from the StruxureWare Data Center Operation
... the StruxureWare Data Center Operation StruxureWare Data Center Operation StruxureWare Data Center Operation (All Versions ... ... that the Apache server (httpd ... files from the server in this state ... ... " from the Operation server using SFTP/ ... In this document, we will be using a free program called WinSCP. You can find this program . Please see the instructions below for a step by step guide for "downloading" files from the server via WinSCP. 1 . Open the application ... 1 . Double click on data folder ... 3. Locate the backup to save off server ... 1 . Double click on /tmp folder
Why isn't my DNS change saving in StruxureWare Data Center Expert?
Changing DNS entries in StruxureWare Data Center Expert UI for VM does not save changes. ... StruxureWare Data Center Expert ... StruxureWare Data Center Expert VM with single NIC configured ... It has been seen where changing a DNS entry in StruxureWare Data Center Expert (DCE) when using the console application does not cause the system to reboot and save the DNS changes. This only happens on a system with a single NIC so it is not seen on the DCE hardware servers , only on a DCE VM server .


Risultati 1 - 10 di 70

Non trovi quello che cerchi?

Contatta l'assistenza clienti per ricevere informazioni, supporto tecnico, assistenza per i reclami e altro ancora.