Sfoglia le FAQ



Where can I get support for APC and MGE Products?
... 50 0031- 10 0031-6 0033- 10 0033-25 ... 6 0034- 1 0034-100 ... 2M- 1 E 0035nd-3M- 1 E 0039-15 0040- 10 0040-15 ... ... 2M- 1 E 0088nd-3M- 1 E 0100- ... 2M- 1 E 0226- ... 3 0377- 1 M 0377- ... 10 0386-12 ... 8 0414- 10 0415-25 ... 50 0467- 10 0467-25 ... 15 0474- 10 0474-100 ...
What are the requirements for the acsc100 condenser unit
... are the requirements for the acsc100 condenser ... ... of rejection of 7 .7kw, ... ... section normally moves up to 1440 m ... ... ; therefore the easiest approach is to ... When the inlet temperature is too low the fans can not slow down enough and then the unit will not control the temperature in the room properly. ... Up to 0.25” (63 kPa) of additional static pressure beyond the standard duct kit installation can be tolerated with only a small impact on the condenser performance.
What are the operational conditions for an InRoom (Stulz) Unit
... the operational conditions for an InRoom ( ... Room Conditions: ... limit: - 10 °C ( ... ... +/- 10 % ... +/- 1 % ... head pressure: 10 bar (145 ... ... 110 kPa ( 10 - 16 psi ... ... Return air conditions for evaporator capacity (DX): 24 °C ( ... ... Return air conditions for cooling capacity (CW): 24 °C ( ... ... (EWT) for CW coil: 7 °C ( ... Leaving water temperature (LWT) for CW coil: 12°C (53.6°F) ... Data is valid for : 460v / 3ph /60 Hz
EcoBreeze Variable Speed Drive Technical Spec’s
... .9 A for 240 V 82.1 A for 200 V , 1 kA ... current 99 A for 60 s Speed range 1 ... ... ... AWG 14 L 1 , L2 ... ... Supply Internal supply for logic inputs at ... ≤ 100 A for overload and short ... Internal supply for reference potentiometer ( ... kOhm) at 10 ... ... 8 V ≤ 10 A for overload and short ... ... Prospective line Isc 1 kA ... with braking resistor for 60 s ... .m L 1 , L2 ...
How do I update/change the language pack on my Network Management Card 2 device?
... 1.1 for Network Management Card ... ... support localization in up to six ... each firmware release for Network Management Card ... ... are also available for download via apc ... ... Below are instructions for updating/changing ... ... different preferred language for all of these ... Only one language pack is ... application for a Smart UPS ... ... labeled language pack for the same version ... ... , please use one of the three ... 2, the easiest method to do ... ... the Device list for a mass firmware ... 1 .) Open ... 7 .) Type ... 10 .) Type ...
Why won't my FM Humidifier Come On?
Room humidity Low, Electrode Carel Humidifier Set- UP , Humid Setup may read Current 0.0A, Conductivity 0micros/cm ... The root cause for this issue is wiring on the back of the humidifier control board have come loose. ... 1 . Check to see if the LEDs are on the humidifier board. 2. Check voltage at P73- 1 , with 100% demand there should be 24 volts there. ... 4. Remove the board and check for loose wires.
Creating an Aggregate Device within the KVM Access Software
... , making it easier for the end user ... ... together to make for ease of management ... ... ports/outlets for a total of ... 1 .) Within ... ... you are adding one of the specifically ... ... information under certain single sign on situations ... ... time to wait for a connection request ... ... click on the one (s) ... ... to enable confirmation for power operation ... to enable delay for power operation, ... 7 .) When ... ... Connectivity page comes up . ... If the server for the aggregate device only has one network interface, ...
NetBotz 450/550/570 | Physical Description
... at start- up , then indicates ... ... = connected at 10 Mbps; orange ... - Flashing one very four seconds ... ... second = Failure 7 Voltage Output Provides 12 VDC or 24 VDC (75 mA) to one connected device. ... Relay Outputs ports 1 ,2 Used for connecting relay- ... Provides 24 VDC (100ma ... ... mA Inputs Provides 24 VDC for connecting third- ... 10 Sensor ports (4) Used for connecting APC by ... ... - 5/ 24 VDC 950ma) ... ... - 5/ 24 VDC (200ma ... ... Rope port Used for connecting a NetBotz ...
How do I upgrade and activate premium devices in StruxureOn?
About Premium ... that are critical for your business to ... get expert assistance for monitoring those devices ... For premium devices, ... 24 / 7 expert monitoring of ... ... a day, 7 days a week enabling remote troubleshooting for quick resolution of ... Incidents are automatically created and tracked, providing easy access to real-time incident status, incident history and chat history. ... Collaborate through chat with Schneider Electric experts for a quick resolution of a problem. Proactive service dispatch ... Connect one device to StruxureOn Premium and you will get analytics and alarms for that device.
What is the time between pump rollovers on Motivair pump packages.
The default settings for both controllers are as follows: ... The changeover timer is set with the buttons on the front of the Easy Relay. Changeover is measured in Hours. To adjust the Changeover timer, press OK, then use the Up or Down arrows to highlight Parameter. Press OK and O 1 is selected. ... The first digit in O 1 is selected. ... Use the Up or Down arrows to adjust the value of the selected digit. ... NOTE: Factory Default Program has a 7 -day (168 hours) pump rotation/changeover timer setting.


Risultati 1 - 10 di 70

Non trovi quello che cerchi?

Contatta l'assistenza clienti per ricevere informazioni, supporto tecnico, assistenza per i reclami e altro ancora.