Sfoglia le FAQ



What are your humidifier specifications and control operations for the InRow RP?
... setpoint and the average return air humidity of all the units in the cooling group (if more than one unit is present).
How many InRow units can be grouped together at one time?
Product Line: All InRow units ACRCXXX, ACRPXXX, ACRDXXX, ACSCXXX
InRow Firmware Upgrade via multiple NMC Cards(ACRC, ACRP , ACSC, ACRD)
NetworkAir, InRow , Firmware, ACRC, ... , ACSC, ACRD, InRow RP , InRow RD, InRow RC, InRow SC,
What is the difference between the leak sensors AP9325 and AP9326?
... is used for the gen1 InRow RC , InRow SC, InRow RD, and ... the gen1 600mm InRow RP , RD, and RC
Why is my ACRP excessively cycling?
The InRow RP works to prevent this by giving an "Excessive Compressor Cycling" alarm. ... If there is empty rack space without blanking panels, the cold air flowing to the hot aisle will reduce the heat load that the RP is given. ... In the Inrow configuration, the supply air setpoint controls the temperature of the air the unit supplies to the cold aisle with compressor control.
What are the minimum load requirements for the ACRP DX?
InRow Cooling ... The InRow RP continually adjusts its cooling output to accommodate varying loads. The cooling output is determined by the difference between the supply air temperature setpoint and the actual supply air temperature as well as the airflow (for each of the cooling units in the cooling group if more than one cooling unit is present). ... At its lowest speed, the equipment cooling capacity is approximately 10 kW but is is recommended to have at least 13 to 15 KW of load per unit .
UPDATED MARCH-2016: Unable to access my APC Network Management Card (NMC) enabled device via HTTPS (SSL/TLS)
... , g50 AV Units , Smart- ... , acrc301s Cooling Units , ... ap9320 Environmental Monitoring Units acrc ACRCXXXX InRow Chilled Water ( ... ... local APC Cooling Support team) g2ats ... ... ACRP5XX, ACRD5XX InRow RC, RP , RD AOS ... ... local APC Cooling Support team) acsc ACSC1XX InRow SC AOS v ... ... local APC Cooling Support team) raru ... Rack Air Removal Unit AOS v3 ... ACRD1XX, ACRD2XX InRow RD AOS v ... ... local APC Cooling Support team) nb200 ... If there are any questions, problems, or concerns related to the content of this article, please contact your local technical support team for further assistance .
What is the difference between an InRow RP, InRow RD (600mm), and InRow RC (600mm)?
These units are the equivalent to an InRow RP with the exception that they do not have the equipment for electric reheat and humidification control ...


Risultati 1 - 10 di 79

Non trovi quello che cerchi?

Contatta l'assistenza clienti per ricevere informazioni, supporto tecnico, assistenza per i reclami e altro ancora.