Sfoglia le FAQ



Where can I find Modbus Register map for Galaxy VX UPS products
Issue: Where can I find Modbus Register map for Galaxy VX UPS products
Where can I find Modbus Register map for Galaxy VX UPS products
Issue: Where can I find Modbus Register map for Galaxy VX UPS products
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
... to take the Single Galaxy 5000 UPS from normal operation ... Galaxy 5000, Galaxy 5500 ... Powering Down the Galaxy 5000 UPS ... power down the UPS are available on ... ... is for a single UPS with an external ... Step 1 : Touch any ... ... “Stop the UPS Step 5 : Press the ... ... protected by the UPS . Step 8 : Unlock CB2 ... The UPS is now fully isolated from the load. ... Step 10 : Turn off the CB3 Input Breaker Step 11: Open the UPS door. Turn off Q 1 Switch ... There is still stored energy in the capacitors, and batteries inside the UPS . Never remove any covers or panels.
Default password of 1234 does not work on the Display of new Galax VX or Galaxy VM.
... of new Galax VX or Galaxy VM. Galaxy VX , Galaxy VM ... display of the Galaxy VX and VM is ... ... cable supplied with UPS Serial port setting: for 9600 bps, 8 data bits, no parity, 1 stop bit, and no flow control. ... Assuming the UPS is connected to the customer network and is granted an DHCP IP address. ... At the bottom of the screen you will a box to enter a password for “Pin [4- 8 digits]” and a “Confirm Pin 4- 8 digits]” and click on Save button.
MGE STS, Galaxy 3000, 4000, 5000 and Galaxy PW; Wiring information for egx100 to any 66061-supported products
... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW ... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW ... for 9600, 8 , N and 1 . Slave address is 1 and wiring is ... ... This assumes only one 66061 card or UPS or STS is ... One is down ( ... ... required on the UPS /STS. The male DB9 connector is not supplied with the UPS but a black terminal block is supplied with the EGX.
Where do I find an Operation Manual for Galaxy VX Series UPS?
Issue: Operation Manual for Galaxy VX Series
Video: How to take the Galaxy 5000 UPS from total power off to normal operation.
Transitioning the Galaxy 5000 UPS from total power ... Galaxy 5000, Galaxy 5500 ... reasons, the Galaxy 5000 may be ... ... commissioning a new UPS . ... of a new UPS must be performed ... ... to restore the Galaxy 5000 UPS from total power ... ... is for a single UPS without an external ... Step 1 : Set the input Q 1 switch to On ... end of the UPS initialization with PFC ... ... “Start the UPS Step 5 : Turn the ... Step 8 : Set the battery circuit breaker(s) QF1 to the On Position. ... The Inverter Assumes the load, and the UPS is normal operation with the load protected.
Galaxy VM Seismic Certification and Anchoring Requirements.
Galaxy VM Seismic Certification ... Galaxy VM ... for documentation regarding Galaxy VM Seismic Certification ... ... the layout or construction of the floor ... Galaxy VM Product Home ... ... -supply- ups -/data ... -phase- ups / galaxy -vm/ N -ecbzda Galaxy VM- 2012 ... Galaxy VM OSHPD pre ... ... -SA- Galaxy VM Typical Seismic ... ... 9GN8T9_R 1 _EN/ Galaxy VM Installation Manual: ... Galaxy VM Seismic Anchoring Document: BYSN-9GN8T9_R 1 _EN Galaxy VM Seismic Certification Document: COCR-9X4HHB_R0_EN


Risultati 1 - 10 di 55

Non trovi quello che cerchi?

Contatta l'assistenza clienti per ricevere informazioni, supporto tecnico, assistenza per i reclami e altro ancora.