Sfoglia le FAQ



What are the computer interface port specifications for the SU and SUA Smart-UPS family?
... G Smart- UPS family? Smart- UPS ... port on the UPS . ... SUA Smart- UPS have the following ... ... RS-232 levels when the UPS signals that it ... The UPS will shut down ... RS-232 level is sustained on pin 1 for 4. ... The UPS responds to this ... (when the UPS is operating on ... Pin 1 is also the ... ... momentary (approximately 1 second) high RS-232 level to pin 7 ... turn on the UPS and any attached ... A momentary low turns off the UPS and its load. ... DC operating voltage is available at pin 8. Smart- UPS Communication
Matrix-UPS run time theory
... method the Matrix UPS calculates its estimated ... Matrix UPS ... on the Matrix UPS calculates the " ... 1 . Age of ... ... applied to the UPS . ... time the voltage levels off for a ... ... To allow the UPS to predict when ... ... curve, the UPS will be able ... ... at 40 volts DC the batteries are ... If the UPS load is too ... that when the UPS is on- ... When the UPS is first installed ... ... Hex) the UPS might begin a ... minimize the inaccuracy on the run time display please refer to the KBase document titled "Requirements for Matrix UPS "Run Time Calibration"
Electrolyte Levels of All Single-phase Symmetra Battery Systems
Issue What are the electrolyte levels of single phase Symmetra UPS and battery systems?
Does the 600mm units have any contact output/inputs?
Yes, it has a form C alarm relay. It also has a single voltage level input (24V AC/ DC nominal).
Matrix-UPS frequently asked questions regarding installation, operation, and standards
1 . Matrix- UPS should be set up on a solid level surface if possible. Padding on floor will help dampen system noise.
Bypass settings of Single Phase Symmetra UPS systems
... voltage is outside of the specified range the UPS will turn off power to the load rather than subjecting it to undesirable voltage levels .
Symmetra PX 250/500; AP9635; Flood of RTC Time adjusted values in the logs
46934 Info IM internal memory for storing configuration settings is OK IO enclosure level 3 pos E ... adjusted value Parallel UPS 1 2 02- ...
3 Phase Products Service Level Agreements; Definition of coverage as relates to the service level agreements offered by SE
Service Level Agreements APC/MGE UPS & PDU ... 3 Phase serviceable UPS / ancillary equipment ... 3 Phase serviceable UPS / ancillary equipment ... relates to the service level agreements offered by ... UPS & PDU On-Site Warranty Extension: ... 1 Site Inspection Visit 1 set of air filters if applicable ... UPS & PDU Advantage Plus: ... 1 Annual PM Visit ... UPS & PDU Advantage Prime: ... 1 Annual Preventive Maintenance Visit ... UPS & PDU Advantage Ultra: ... 1 Annual Preventive Maintenance Visit 1 Set of air filters if applicable ... TSE agent will follow internal protocol to handle the service coverage and necessary actions to process customer requests per SLA.
What are the various generations of Smart-UPS Products?
... various generations of single phase Smart- UPS Products? Smart- UPS ... of Smart- UPS products in use ... ... is a high level overview, and ... ... for your specific UPS . Current Products: ... Interactive Smart- UPS products ... Serial Port on UPS ) ... Interactive Smart- UPS products ... Serial Port on UPS ) ... generation Entry- Level Line Interactive Smart- UPS products 1kva - 1 .5kva ... Serial Port on UPS ) ... Designed for entry level server and Small ... ... Interactive Smart- UPS (Similar to ... 1 .5kva - ...
Video: SRT UPS reports Battery Charger Event, Event Code 142
The UPS reports: Battery ... 142 on the UPS LCD display or ... SRT UPS Models With the UPS input connected to ... ... the appropriate SRT UPS model to disconnect ... Using the UPS LCD display, ... the appropriate SRT UPS model to navigate the UPS LCD menu. ... measurements on the UPS charger or battery ... ... displayed on the UPS LCD display is ... the “Voltage level ” (refer ... blown and the UPS requires replacement. ... displayed on the UPS LCD display is ... the “Voltage level , the batteries ... Voltage level ... Li-Ion 1 - 1 .5kva If ...


Risultati 1 - 10 di 82

Non trovi quello che cerchi?

Contatta l'assistenza clienti per ricevere informazioni, supporto tecnico, assistenza per i reclami e altro ancora.