Sfoglia le FAQ



Treck TCP/IP Vulnerabilities (ripple20)
To stay up to date on security ... , please register for Schneider Electric Cybersecurity ... UPS Network Management Cards ... (SmartSlot, pre -installed with Smart- UPS , Symmetra, ... 3500, SUVT UPS , 3-phase Smart- UPS & Symmetra UPS ) ... include Smart- UPS , Symmetra, Galaxy UPS , Metered/ ... ... upgrade, links to the various applications ... ... is dedicated only to provide APC Network ... ... will be added to the table as ... For support on performing ... ... scanning software detects for the presense of ...
APC UPS Network Management Card (NMC) Compatibility Chart
... Which model of UPS Network Management Card ... supported in my UPS ? UPS Network Management Card ... UPS Network Management Card ... UPS Network Management Card 1 - AP9617, ... UPS Web/SNMP ... ... has been created for reference. Please refer to the table below ... ... compatibility between current UPS models and discontinued ... cards, support for new device features ... Network Management Card for your device. ... application file, for use with the Smart- UPS family. Firmware files for use in other UPS systems can be ... UPS Model Single and Three Phase Smart- UPS with the following ...
Questions on where to ship 3 phase batteries for disposal
... Questions on where to ship 3 phase batteries for disposal For disposal of batteries ... Schneider only provides pre -paid shipping labels for batteries that are ... under their initial 1 year warranty or for batteries being replaced ... a specific battery contract . ... Customers are welcome to ship batteries to the following address for proper disposal of ... For all 3 phase ... customer is required to pay for the return ship ... specific Battery Service contracts . Customers may arrange their own heavy weight pick up if desired thru major shipping companies. Schneider does not provide packaging for returning batteries.
How to set self test day and time on Symmetra UPS products
How to set self test ... time on Symmetra UPS products ... reset the counter for the self test ... 1 ) A UPS load on command ... ... ) An adjustment to the self test ... ... your self test to run every two ... ... (esc) to main UPS menu ( up /down) change to never (enter ... ... again) change to 14 days ( ... Your UPS self test should ... ... 100, 160 kVA the menu path ... UPS -> UPS Configuration -> ... ... that anytime the UPS is commanded on ...
Stacking limitations for single phase Symmetra and Matrix products
The UPS and batteries can be stacked up to 62" high. Possible configurations include:
Matrix-UPS emits a chirping sound after being on-battery or running a self-test
... pack fails a UPS On-Battery ... scheduled or through UPS start- up ), the Matrix- UPS will emit chirps for an interval of one minute to warn of a ...
What are the computer interface port specifications for the SU and SUA Smart-UPS family?
... interface port specifications for the 3G Smart- UPS family? Smart- UPS ... by connecting directly to the serial port on the UPS . ... SUA Smart- UPS have the following ... ... must be pulled up to a common referenced ... greater than + 40 Vdc. ... generates a low to high transition at ... levels when the UPS signals that it ... The UPS will shut down ... sustained on pin 1 for 4.5 ... The UPS responds to this signal only ... (when the UPS is operating on ... Pin 1 is also the ...
AOS v6.3.2/sy3p APP v6.3.2 UPS Network Management Card 2 (NMC2) ap9630/AP9631 UPS Compatibility
... v6.3.2 will provide support for Symmetra PX 20, 40 , 80 kVA models only (especially to help address ...
How to configure the SRC 5,6,8 & 10 KVA UPS Models External Battery Packs using the LCD display
The 80ah inside the table is the default setting for 5kva/6kva ( 1 EXB: 16pcs of 5ah battery)
INFORMATION BULLETIN - Interface Expander 2 SmartSlot Card Smart Signalling Information and Explanation
For most newer generation UPS devices, DIP ... be in the 1 ( up ) position. ... Expander 2 waits for all "connected clients" to signal shutdown before commanding the UPS to shutdown.


Risultati 1 - 10 di 77

Non trovi quello che cerchi?

Contatta l'assistenza clienti per ricevere informazioni, supporto tecnico, assistenza per i reclami e altro ancora.