Consulter la FAQ



Refrigerant charging table for a Uniflair Unit
• Use the formula: Total Equivalent length = Vertical line length + Horizontal line length + Equivalent Length of Fittings
How do you install an Isolated Extension Cable with a Share-UPS?
Issue Need assistance on installing the Isolated Extension Cable ( IEC ) with a Share UPS.
Using the 940-1524 Smart Signaling Cable and UPS Interface Extension Cables
The Network Enhancements division has developed an Isolated Extension Cable ( IEC ), APC part number ... ft.) of total cable length .
Why would I need to use the 24VDC adapter when using the APC Isolated Extension Cable?
... through an Isolated Extension Cable ( IEC ), you must use a 24VDC adapter to power the UPS End Unit of the IEC .
Do I need to use a 24VDC power adapter with the Isolated Extension Cable?
... through an Isolated Extension Cable ( IEC ), you must use a 24VDC adapter to power the UPS End Unit of the IEC .
What are the main difference between the ap9550, AP9551, AP9553, AP9554, and the AP9555 Rack Power Distribution Units?
Max Amperage Draw AP9551 Vertical ... IEC Outlet IEC Outlets ... AP9554 Vertical IEC Outlet IEC Outlets
Can the finger-style vertical cable managers for 600 mm cabinets be installed on the same 0U Accessory Channel as a PDU?
Issue: Customers may want to mount a PDU on the accessory channel behind the vertical cable manager.
What is the maximum kW rating for the NetShelter SV?
The SV is not compatible with most of the datacenter architecture and accessories such as EcoAisle containment, Vertical Exhaust Duct and InRow.
How can an IEC 320 International Standardized Appliance Connectors, and it's gender, be identified?
5) To extend the length of an existing cable requires a male to female cable.


Résultats 1 - 10 de 81

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.