Consulter la FAQ



What is the difference between an InRow RP, InRow RD (600mm), and InRow RC (600mm)?
The minimum required kW for 1 direct expansion unit is 12kw and 12kw for chilled water. There should also be a consideration regarding humidity control.
Network Air FM unit spare parts list
ADAPTER ROTO 1 1 /4" ... ADAPTER ROTO 1 "-14R ... "SWT ( indoor rec'r) CAT5 for EXP unit ... - MKC- 1 ... ASSY FM 35 KW DX ... ASSY FM 40 KW DX ... ASSY FM 50 KW DX ... compressor [K 1 & K2 ... ... DF 5/ Unit 756 X 325 ... ... DF 5/ Unit 756 X 325 ... ... FM35-50 KW W/AIR ... ... FM35-50 KW W/AIR ... ... FM35-50 KW W/AIR ... ... FM35-50 KW W/AIR ...
How to install a Remote On/Off (EPO) in a Uniflair unit.
The following figure represents one of the most common diagrams for connecting the 24 Vac digital inputs, for a pco3.
EcoBreeze Variable Speed Drive Technical Spec’s
Motor power kW 15 kW ... .9 A for 240 V 82.1 A for 200 V , 1 kA ... current 99 A for 60 s Speed range 1 ... ... ... AWG 14 L 1 , L2 ... ... Supply Internal supply for logic inputs at ... ≤ 100 A for overload and short ... Internal supply for reference potentiometer ( ... ≤ 10 A for overload and short ... ... Prospective line Isc 1 kA ... with braking resistor for 60 s ... .m L 1 , L2 ... ... AI3 8 ms for analog LI1. ... LI6 4 ms for discrete
ACSC1XX Spare Parts List
... Spare Parts List for ACSC1XX units . 1 ... 12 BLK ( for baying kit) BOX ASSY for DUCT KIT ACSC ... 1 1 1 1 ... Ceiling Tile Adapter 24 " - Spare ... ... -230/ 1 /60 ( ... ... -240/ 1 /50 ( ... ... -230/ 1 /60, ... 1 ... -240/ 1 /50 SC ... 1 ... -4367 ( for Dual Condensate Pump ... ... -4368 ( for Dual Condensate Pump ... ... long PVC TUBE for 875-4367 ... ... -0481 ( for Dual Condensate Pump ... ... long PVC TUBE for 875-4368 ...
Modbus Register Map for Gen 1 600mm InRow Units
Issue: Modbus Register Map for Gen 1 600mm InRow Units
Refrigerant charging table for a Uniflair Unit
... Refrigerant charging table for a Uniflair Unit . ... -cooled DX units must be connected ... Systems with remote outdoor ... ... failures due to system vibrations. ... the following table for reference when determining ... ... oil throughout the system , in particular ... For pipes running in ... ... determine pipe diameter for vertical pipes. ... determine pipe diameter for horizontal pipes. 1 . Open any ... present in the system to ensure that ... ... . Pressurize the system to 17. ... ... . Leave the system pressurized for 24 hours. ... leaks from the system , perform the system evacuation. System Evacuation:
How to set up group communications for an Network Air FM unit
In a system one of the modules is designated by ... the rest of modules in the systems are identified as “Expansion Modules”.
What are the placement considerations for the fluid cooler relative to the InRow acrd20x?
The longer the distance of the fluid cooler from the indoor unit , the larger the size of the pump required.
What are the placement considerations for the condenser relative to the InRow RD? What are the other factors involved with purchasing a fluid cooler?
The longer the distance of the fluid cooler from the indoor unit , the larger the size of the pump required.


Résultats 1 - 10 de 90

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.