{}

Consulter notre FAQ

{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}

NetBotz 755 supports up to 4 AP9520T/TH sensors

Issue:
NetBotz 755 manual incorrectly states 12 AP9520T/TH sensors supported

Product Line:
NetBotz

Environment:
NBWL0755

Cause:
An incorrect notation in the initial NetBotz 755 manual states that up to 12 AP9520T or AP9520TH A-link sensors are supported

Resolution:
The NetBotz MBWL0755 only supports up to 4 AP9520T or AP9520TH A-link sensors and the manual is incorrect. The manual will be changed but in the meantime, we've added this FAQ to hopefully limit confusion.

Cela vous a-t-il été utile ?

En savoir plus
En savoir plus