FAQs durchsuchen

What do I gain with a Unity Output Power Factor (kW=kVA)?

Veröffentlichungsdatum: 24 January 2018

 
Issue:
What do I gain with a Unity Output Power Factor (kW=kVA)?
 
 
Product line:
Three Phase UPS Systems
 
 
Environment:
All models/ all serial numbers
 
 
Cause:
What do I gain with a Unity Output Power Factor (kW=kVA)? The advantage of unity power factor is that these UPS systems are 100% compatible with today's high power factor loads. Traditionally, a UPS with a lower power factor needs to be oversized to support today's power factor corrected loads.  Some APC 3-phase UPS products as well as newer single phase products(SRT6K) have an output rating of kW=kVA or Unity Power Factor. While the more traditional double conversion units have output ratings of kW=0.8kVA. 
 
 
Resolution:
Refer to the following application note for a better understanding of power factor as related to APC products

https://www.apc.com/salestools/SADE-5TNQYL/SADE-5TNQYL_R1_EN.pdf
 
 

War dies hilfreich?

Was können wir tun, um die Informationen zu verbessern?

Nicht gefunden, was Sie suchen?

Wenden Sie sich an unser Kundenteam, um Informationen zum technischen Support, Unterstützung bei Beschwerden und vieles mehr zu erhalten.