FAQs durchsuchen



Galaxy 3500, Smart-UPS VT and ais3000 Power Factor Information
Galaxy 3500 , Smart-UPS VT and ais3000 Power Factor Information ... Galaxy 3500 , Smart-UPS VT and ais3000 ... Galaxy 3500 , Smart-UPS VT and ais3000 Power Factor Information ... "The SUVT and the ais3000 have an Input Power Factor Correction Module which corrects the Power Factor on the input of the unit. The Input Power Factor is 1 . The Output Power Factor is 0.8 - what means that, for example, a 10kva unit can provide a maximum total load of 8KW. This means there is a difference of 20 % between real and apparent power.
Batteries; Is it OK to replace the internal batteries or use refurbished modular battery modules?
Symmetra PX1 20 - 80 kva , Symmetra PX2 100 kva , Symmetra PX 250-500 kva , SUVT , g3500, ais3000, Galaxy VM
Smart-UPS VT, Galaxy 3500; What is Cyclic Charge Mode?
Smart-UPS VT, g3500, What is Cyclic Charge Mode, Cyclic Charge Mode, SUVT , Galaxy 3500 , ais3000
How do I connect a EPO circuit to Smart-UPS VT or Galaxy 3500 Battery XR Frame?
Galaxy 3500 , SUVT , EPO, REPO, g3500, Battery frame, XR frame, XR frame EPO circuit wiring, Installation – ...
​Video: How to Remove the Battery Blanking Panel on a Galaxy 3500 and Smart-UPS VT UPS
Galaxy 3500 , SUVT , Blanking Panel, Operation, Video,Smart-UPS VT UPS
Which SmartSlot accessories are supported by the Galaxy 3500 (g3500) UPS?
g3500, galaxy 3500 , SUVT , accessories, MGE g3500, MGE galaxy 3500 , SmartSlot accessories, AP9622, modbus
AP9622 Modbus uses MTU (NOT RTU)
AP9622,RTU,MTU,Modbus, SUVT , Galaxy 3500
What UPS units are officially supported by the ap9610 (Relay I/O SmartSlot Card)?
SURTA SUVT / Galaxy 3500 (Must use Configuration #2 - same as Symmetra)
What UPS units are officially supported by the AP9613 (Dry Contact I/O SmartSlot Card)?
SURTD SUVT / Galaxy 3500 (Must use Configuration #2 - same as Symmetra)


Ergebnisse 1 - 10 von 58

Nicht gefunden, was Sie suchen?

Wenden Sie sich an unser Kundenteam, um Informationen zum technischen Support, Unterstützung bei Beschwerden und vieles mehr zu erhalten.