How can I adjust the number of battery packs on a Smart-UPS XL?
All models , All Serial ... : Models that begin with ... are not XL models , even though ... ... -UPS XL models are not designed ... ... -UPS XL models are not designed ... ... runtime calculations which a Smart-UPS ... 1 . Using Hyperterminal ... ... battery packs via a Hyperterminal session: 1 . First, ... ... asked to choose a name and select ... If a message appears which ... .must install a ... 2400 baud, 8 data bits, 1 stop bit, ... 5 . Click on ... a . Type " ... ( A new unit will ... ... "" Adds a battery pack