EcoBreeze Variable Speed Drive Technical Spec’s
Product specific application Simple machine ... 200 V , 1 kA Speed range 1 ... ... ... AWG 14 L 1 , L2 ... ... kOhm) at 10 ... ... 8 V ≤ 10 A for overload ... ... Prospective line Isc 1 kA ... .m L 1 , L2 ... ... ... 10 V , input ... +/- 10 V , ... ... 10 V , impedance ... ... V (state 1 ) LI1. ... ... V (state 1 ) ... configurable relay logic 1 NO + 1 NC , electrical ...