FAQs durchsuchen
Electrolyte Levels of All Single-phase Symmetra Battery Systems
Issue
What are the electrolyte levels of single phase Symmetra UPS and battery systems?
Product Line
Symmetra Power Array
Symmetra RM
Symmetra LX
Environment
All serial ranges
Cause
This document contains the electrolyte levels found in the battery modules used by each single phase Symmetra system. This information can sometimes be needed for regulatory compliance in certain jurisdictions.
Resolution
Symmetra Power Array
SYBATT: Each SYBATT contains (10) 12V 7.2Ah batteries installed in series. The total amount of electrolyte in (1) SYBATT is 0.845 gallons.
Symmetra 12k RM
SYBT3: Each SYBT3 contains (10) 12V 7.2Ah batteries installed in series. The total amount of electrolyte in (1) SYBT3 is 0.845 gallons.
Symmetra 6k RM
SYBT2: Each SYBT2 contains (10) 12V 5.1 Ah batteries installed in series. The total amount of electrolyte in (1) SYBT2 is 0.55 gallons.
Symmetra LX
SYBT5: Each SYBT5 contains (10) 12V 9Ah batteries installed in series. The total amount of electrolyte in (1) SYBT5 is 0.95 gallons.
Veröffentlicht für:APC Switzerland
Weitere Produktinformationen
Bereich:
Weitere Produktinformationen
Bereich: