Rack PDU 2G (AP8XXX) Network Port Sharing Information
... Capability of AP8XXX Rack PDU models Rack Power Distribution AP8XXX Rack PDU series only ... up to four Rack PDUs using only ... ... by connecting the Rack PDUs via the ... ports on the Rack PDU front panel ... All Rack PDUs in the ... using the same Rack PDU firmware revision ... ... uniquely identify the Rack PDUs in a ... ... two or more Rack PDUs are connected ... ... viewable on the LCD by selecting the ... option on the LCD keypad. ... up to four Rack PDUs. ... or AP89XX series Rack PDU was manufactured ... ... are available from APC . Please contact ...