Consulter la FAQ



This document describes how the Magnum VS DC Power shelf operates when the controller card is removed.
The Controller card on the Magnum VS stores the user settings , should this card become faulty it can be ‘hot-swapped’ ...
Video: How to configure redundant group control for a DG4 or DG5 controller
Set all other Trm# to none Scroll to Ok? with the enter key and change it to Yes then hit enter.
BMS AP9921X-AP9922; what specific alarms will set the “Management Controller Alarm?
... the “Management Controller Alarm?” ... the “Management Controller Alarm?” ... activate the Management Controller LED. ... this alarm, it inhibits relay scanning ... ... the charger is functioning correctly. It is possible to ... a standard CAT5 data cable to interconnect ... One or more connections between the Management Controller and the batteries are open. ... The surface temperature of one battery in the string is above the configured threshold. ... The connections between the Management Controller and the batteries are open.
What is Modbus and How does it work?
... used for transmitting information over serial lines ... ... device requesting the information is called the ... devices supplying information are Modbus Slaves ... ... can also write information to the Slaves ... What is it used for? ... , meaning that it's free for manufacturers ... It has become a ... It is used widely ... to a main controller or data gathering system, ... ... supervisory control and data acquisition (SCADA ... How does it work? The data is sent as ... ... troubleshooting problems, it can be helpful ... the actual raw data being How is data stored in Standard ... Information is stored in ...
What does the "Reset ATS Controller" command accomplish on a Next Gen Rack Automatic Transfer Switch (ATS)?
... "Reset ATS Controller " command accomplish ... This information is provided to ... "Reset ATS Controller " command does and the functions it performs. ... resetting the ATS controller through the Network ... ... Resetting the ATS controller will cause the ... the ATS preference settings . When you reset the ATS controller , the ATS will switch to source A and remain on source A. Why? ... When you reset the ATS controller , the ATS will switch to source A and approximately 30 seconds later switch back to source B Why? Source A is the default source selection.
How do I mass configure APC user settings using Data Center Expert?
NOTE: If the user already exists on any destination device, all its settings , including the password, will be overwritten.
NetworkAIR Legacy Dataguard 5 Common Alarm Facts
Data Center Cooling ... NC on the controller board. ... button >> Config . ... column, then it will generate a ... ... column, then it will not generate ... ... to same state it was before the ... :If the AC is powered off after being on from the On-Off button on the display, this will generate a common alarm while it is off if the KEYPAD OFF event is set to "ON" in the "COM" column in the Alarm Menu section.
Uniflair BACnet (Building Automation and Control Networks)
This document describes the operation of the Uniflair BACnet (Building Automation and Control Networks). ... To realize a local net to be connected to a BMS with protocol BACnet, it’s necessary: ... • 1 RS485 serial card for every controller ; ... • PC for the gateway configuration ... These are the ways how the information under BACnet can be sent to Uniflair controllers :
How to navigate through an Network Air FM unit display
Operation . System Configuration The System configuration options are defined ... Changing the settings incorrectly can cause ... ... changes to these settings . Some System configuration settings may not apply ... ... # > System Config > System Options menu contains settings that identify the ... The configuration is based on ... ... Indicates the coil configuration installed in the ... This setting controls the number ... A setting of zero indicates ... Use this setting if you are ... ... # > System Config > System Delays It protects the compressors ... It protects the compressors ... It prevents a second ... ... System cannot begin operation until this delay ...
What is the VFD RS485 Communication Error on my NetworkAIR FM/ir40?
Data Center Cooling "In controller firmware v6 ... The FM controller continuously polls data from the VFDs, one data point at a ... ... each piece of data . ... if the FM controller receives either an ... ... one piece of data reaches the value ... The alarm is cleared when the error counts of all data items have a value of zero. ... It is also possible that one or both VFDs have the wrong address programmed into them. To check this you'll need to connect the VFD keypad to each VFD and check the value of parameter H31.


Résultats 1 - 10 de 92

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.