Consulter la FAQ



"Battery Predicted Replacement Date" missing from ap9630/31 UPS Network Management Card 2 (NMC2) Web Interface on supported UPS models
... support "Predicted Battery Replacement Date" or " Battery Predicted Replacement Date ... or "Next Battery Replacement Date" ... command or via SNMP OID .iso.org.dod.internet.private.enterprises. apc .products.hardware.ups.upsBattery.upsAdvBattery.upsAdvBatteryRecommendedReplaceDate (.1.3.6.1.4.1.318.1.1.1.2.2. 21 ). ... SNMP OID requires APC PowerNet MIB v4.0.8 or higher.
How do I recycle APC batteries in the US and Canada?
Issue: How do I recycle APC batteries in the US and Canada?
What is the expected life of my APC UPS battery?
Most APC batteries should last three to five years. There are many factors which affect Battery life including environment and number of discharges.
Why should I use only genuine APC Replacement Battery Cartridge (RBC) in my APC UPS?
Using of a non- APC battery may result in lower runtime, damage the UPS, create hazardous conditions, or void safety certifications ...
Why aren't alarms clearing in the BMS (Battery Management System) AP9921X-AP9922 after replacing batteries?
After changing a battery in a string which is monitored by the APC Battery Management System, it is imperative to clear the old baseline ...
Complying with U.S. Department of Transportation (DOT) Shipping Regulations for Sealed Lead-Acid Batteries
All the batteries APC ships meet the requirements of UN Number 2800 ("" Batteries , wet, non-spillable"") ...
Video: What to do if the system is missing native shutdown battery options / How to restore HID UPS device driver.
... HID driver (Human Interface Device) being updated from HID UPS to APC UPS or APC Battery BackUP.
Battery Discharge During Storage
APC Batteries should be charged to 100% within 6 months of purchase by the end user.
What are the Minimum and Maximum mounting depths for Smart-UPS rails?
This includes the UPS as well as any associated external battery packs. ... For specifics of how to mount your unit, please refer to the installation documentation included with your UPS or External Battery Pack. ... The minimum depth for the rails is 21 .75" and the maximum depth is 36". ... If you are using your APC rail kit to mount non- APC equipment your experience may vary.


Résultats 1 - 10 de 96

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.