Consulter la FAQ



How to configure the SRC 5,6,8 & 10 KVA UPS Models External Battery Packs using the LCD display
... 16 pcs of 100 AH batteries in series(for 5 KVA ), the total AH number is 100 AH x 16 pcs= ...
Smart-UPS SRC 5k, 6k, 8k and 10 KVA FAQ
SRC 5 ,6, 8 and 10 KVA FAQ ... Do the SRC 5 -10 KVA UXI Models turn ... ... taken out of service for maintenance) ... ... of the SRC 5 -10 KVA LCD Display? ... input/output voltage , input/ ... , and battery voltage , etc.,The Output Voltage can be set ... ... /6/ 8 /10kvauxi Models ... ... 6A/ 8 A, in ... ... to choose a Service Bypass Panel? ... +1 Parallel redundancy system, the ... look into a service bypass panel which ...
NetBotz 750 | Configuring Network Settings
Process for configuring network settings on NetBotz version 5 appliances. NetBotz version 5 ... - Rack Monitor 750 NetBotz v 5 . X Establish Network Settings You must configure the following TCP/IP settings before the appliance ... ... use DHCP to configure network settings automatically, or ... terminal emulator to configure network settings manually. ... to Establish Network Settings ... uses Dynamic Host Configuration Protocol (DHCP) to configure network settings . ... to Establish Network Settings ... the following connection parameters : ... Data Bits: 8 The terminal settings are correct as ... 5 ) Log on ...
NetBotz 750 | How do I connect serially?
... to the NetBotz 750 ? NetBotz version 5 . X NetBotz v 5 . X Serial parameters and drivers are ... The NetBotz 750 uses the following serial parameters : ... - Data Bits: 8 ... To log in and configure the 750 with an IP, you will need to log in with root as the user and you will be prompted for a password. If you connect your NetBotz 750 to your computer and do not see it show up as a serial port (unknown device), you need to download the driver:
Video: Data Center Expert | How do I configure the network settings?
Network settings configuration on a StruxureWare ... ... that the network settings (IP Address ... ... Editing the Network Settings will cause the ... ... design, network settings for Data Center ... Configuration of Network Settings on the DCE ... ... Prompted and within 5 seconds, press enter to change settings . ... to modify the settings . 5 ) Set the ... ... to display network settings only (DCE ... 8 ) If desired ... or disable n [enter] 5 ) After the ... First Configuration of Network Settings on the DCE ... 5 ) When Prompted and within 5 seconds, press enter to change settings .
NetBotz 750 | Resetting a Lost Root Account Password
... accessing the NetBotz 750 via console or ... NetBotz version 5 ... - Rack Monitor 750 NetBotz v 5 . X ... emulator using port settings : ... Data Bits: 8 The terminal settings are correct as ... ... a key within five seconds after you ... 5 ) Enter the following three commands: ... If you do not press a key within 5 seconds after you connect power to the appliance, the appliance will restart normally. 8 ) Enter the following three commands: ... NOTE: If you do not complete steps 7 and 8 , the root password will be reset every time the appliance restarts.
NetBotz 750 | What parts come with the NetBotz 750?
... NetBotz Rack Monitor 750 1 2 Wireless ... , M4 x 8 4 5 2-position ... block plug 1 8 tie wraps, 203 mm ( 8 in) 2 ...
UI throws 503 error after restoring a backup to a NetBotz 750/755 from another NetBotz appliance
... to a NetBotz 750 /755, ... System settings may become corrupt ... 1. Configure all system settings ... that is already configured . 5 . Restore the ... ... to defaults and configure the IP serially ... ... micro USB serial configuration cable. ... use the following settings and connect with ... 8 Data Bits ... Log in using root and the password you had provided upon initial root login (done via serial connection), then when prompted to press enter within 5 seconds, type a capital X and hit Enter.
Netbotz 700 Series | How can I reset the NetBotz 750 to defaults?
... NetBotz Rack Monitor 750 (nbrk0750) NetBotz Version 5 appliances ... press enter within 5 seconds, type a capital X . At the ... ... micro USB serial configuration cable. Once connected, verify you're using the correct port in device manager, then use the following settings and connect with a terminal emulation program such as Hyper-terminal or Putty: ... 8 Data Bits ... Log in using root and the password you had provided upon initial root login (done via serial connection), then when prompted to press enter within 5 seconds, type a capital X and hit Enter.
NetBotz 750 | Physical Description
... of the NetBotz 750 NetBotz version 5 ... - Rack Monitor 750 NetBotz v 5 . X ... connected device when configured events occur. ... outlet may be configured to turn on ... standard CAT- 5 cabling with straight ... ... Installation and Quick Configuration Manual. 5 Rack Access Ports ... ... party 0- 5 V sensors. ... , 0- 5 V sensors require ... NetBotz 0- 5 V sensor cable ... 8 10/100/1000 Network Port Provides a connection to the network. ... 13 Voltage Output Provides 12 VDC or 24 VDC (75 mA) to one connected device.


Résultats 1 - 10 de 84

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.