Consulter la FAQ

Can a 3rd party UPS be installed in the AR106V or AR106VI?

Date de publication : 23 October 2019

Issue:
It is unknown if a 3rd Party UPS can be installed into the AR106V and AR106VI. 


Product Line:
AR106V, AR106VI

Environment:
All versions and serial ranges.

Cause:
The NetShelter WX 6U Vertical cabinets have a mounting bracket for a 2U UPS. 

Resolution:

Any 3rd party UPS must be validated by the manufacturer to work with this cabinet prior to installation:  
The manufacturer must validate that the 3rd party UPS can be installed vertically. Not all batteries can install in this orientation. 
When shipping with a 3rd party UPS installed, the manufacturer must validate that the 3rd party UPS can ship installed using their rail kit(s), without disconnecting in transit. 

 

Cela vous a-t-il aidé ?

Que pouvons-nous faire pour améliorer l'information ?

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.