MGE STS, Galaxy 3000, 4000, 5000 and Galaxy PW; Wiring information for egx100 to any 66061-supported products
... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW egx100 and all products supported by 66061 – STS, Galaxy 3000, 4000, 5000 and Galaxy PW ... Resolution : ... The 66061 JBUS/Modbus card is configured for 9600, 8, N and 1 . Slave address is 1 and wiring is 2-wire with no parity and termination. This assumes only one 66061 card or UPS or STS is connected to the enclosure but if more than one change as required. ... One is down (off position) and all others are up.