Consulter la FAQ



My Micro DC came with clamp-on ferrites. Where do they go, and are there installation instructions?
Cause: The Micro Data Center SX International units ship with one snap-on ferrite per piece of installed equipment.
Matrix-UPS run time theory
1 . Age of ... ... fully charged battery begins to discharge ( ... ... time the voltage levels off for a ... A calibration might establish that at 40 volts DC the batteries are 2 minutes from reaching 39 volts (which is always the end of discharge). ... When the UPS is first installed with a brand new set of batteries, this constant is set to a Hexadecimal value of "B0". ... If the constant is too low (below "80" Hex) the UPS might begin a graceful shutdown too soon or show an abnormally short run time.
ACSC1XX Spare Parts List
1 1 1 1 1 ... -230/ 1 /60 ( ... ... -240/ 1 /50 ( ... ... -230/ 1 /60, ... 1 ... -240/ 1 /50 SC ... 1 ... JUMPER (for activation without the water ... 1 1 DC RECTIFIER, 500 ... 1 1 1 1 ... WASHABLE IR SERIES 1 /2" ... FITTING 1 /8" ... FITTING 1 /8" ... 1 ... BULKHEAD MOUNT ( single float) 1 1 FOOT LEVELING m10 X 51 ... 1
Video: Troubleshooting no communication between UPS and PowerChute Business Edition
Troubleshooting Windows Serial Communications ... as the baud rate for Smart- ...
Does the 600mm units have any contact output/inputs?
Yes, it has a form C alarm relay. It also has a single voltage level input (24V AC/ DC nominal).
NetBotz 355 | Physical Description
- Flashing one very four seconds ... ... When the unit first receives power, displays the unique identifier number for one minute. ... at the same rate as the Alert ... ... focus of the integrated camera. 1 Sensor ports ( ... - Status LED: blinks orange and green at start -up, then indicates the status of the network connection (solid green = IP address established; blinking green = attempting to obtain an IP address).
NetBotz 455 | Physical Description
- Flashing one very four seconds ... ... When the unit first receives power, displays the unique identifier number for one minute. ... at the same rate as the Alert ... ... focus of the integrated camera. 1 Microphone jack Supports audio sensing, audio recording, and two-way audio. ... - Status LED: blinks orange and green at start -up, then indicates the status of the network connection (solid green = IP address established; blinking green = attempting to obtain an IP address).
NetBotz 300-500 Series | Configuring Email Notifications
NetBotz v3 Rack Appliance: 450/451 (nbrk0450/ 1 ), 550 (nbrk0550), & 570 (nbrk0570) ... Select First Alert Level (can be modified) and click Edit ... Select Sensor Pod that requires modification (default is Sensor Pod integrated ) and click Sensors
Description of Matrix-UPS charging circuit
There are also two types of charge levels. The first one is called a constant current rate of charge.
SRT 8 or 10kva reports Error P.11 or DC Bus Soft Start or event codes 124/125
1 . Improved system performance of transitions between Online and Bypass operation modes.


Résultats 1 - 10 de 83

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.