Consulter la FAQ



Frequently Asked Questions (FAQs) for UPS Network Management Card 2 (NMC2)
Is UPS NMC 2 compatible with all single phase SmartSlot UPSs Does UPS NMC 2 integrate with StruxureWare Data Center Expert and InfraStruxure Manager?
Data Center Expert | Why does the trap I received omit the argument for sensor ID?
StruxureWare Data Center Expert NMS integration feature. 7.x and prior.
Why does StruxureWare DCE show duplicate sensors after upgrade, one of the duplicates reports unplugged.
StruxureWare Data Center Expert. ... StruxureWare Data Center Expert any version DDF files for StruxureWare ... During the upgrade of StruxureWare , many DDF files are often updated. ... Changes to sensor IDs within the DDF are at times necessary in order to better integrate the sensor information with external systems such as StruxureWare Data Center Operation. ... Please be aware that in either case , deleting the device (all data lost) or deleting the sensor itself (old sensor specific data) will cause the loss of data.
Netbotz Advanced View | Does NOT Support Radius, Active Directory or LDAP
NOTE: NetBotz Central, ISX Central, and StruxureWare Data Center Expert do support integrating with both Active Directory & OpenLDAP remote authentication server ...
What type of information is provided in an SNMP trap from StruxureWare Data Center Expert?
StruxureWare has the ability to send traps using the "Alarm ... " functionality as well as the "Network Management System Integration " feature.
Can StruxureWare Data Center Expert be configured to alert for NetBotz 3xx, 4xx, and 5xx devices?
Ever since their integration with NetBotz Central, NetBotz devices were designed to alert for themselves.
Can StruxureWare Data Center Expert output a 32 bit register with its Modbus output?
DCE will output 65535 but your BMS will need to divide by 10 in such cases .
Data Center Expert | How do I enable SSL communication between StruxureWare and multiple Netbotz devices?
integration , swc, isxc, dce, cert, ssl, netbotz, botzware, bot, certificate, ssl
Are there any StruxureWare DCE version limitations to newer Dell servers now used ?
StruxureWare DCE versions may be limited by newer hardware ... StruxureWare Data Center Expert ... In some cases , newer drivers may be necessary.


Résultats 1 - 10 de 56

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.