What are some features I need to be aware of while manipulating the config.ini file of a APC Network Management Card?
... Network Management Card 1 (NMC1) ... Devices with an embedded Network Management Card 1 include (but are not limited to): Metered/Switched Rack PDUs (AP78XX, AP79XX), Rack Automatic Transfer Switches (AP77XX, Environmental Monitoring Units (ap9320, ap9340, Netbotz 200) ... Firmware versions v3. X . X and higher ... =00 C0 B 7 6A 33 56 ... These values are protected to avoid accidently setting the same potentially "site specific" settings to multiple UPSs without extra care , just as with the TCP/IP settings.