{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}
{}

Nos marques

{"support":{"yesButton":"Oui","noButton":"Non","feedback":{"title":"Quelles améliorations pouvons-nous apporter ?"},"submitButton":"Soumettre","successMessage":"Merci de nous avoir fait part de vos commentaires.","title":"Cela vous a-t-il été utile ?","feedbackPercentLabel":"personnes ont trouvé cela utile","captcha":{"error":"Veuillez cocher la case appropriée."}}}
Consulter notre FAQ

DCO | Can more than one client instance be running on the same computer?

Issue:
Can more than one (1) instance of a Data Center Operation desktop client be used on a computer at the same time?

Product Line:
StruxureWare Data Center Operation (DCO)

Environment:
StruxureWare Data Center Operation (all versions)

Cause:
When attempting to load more than one DCO desktop client on the same computer an error message appears displaying, "There is another application instance started by the current user and the workspace directory is currently in use."

Resolution:

Only one instance of the DCO Desktop Client can be opened at a time.  This is by design and there is no work around for opening more than one client on the same computer at the same time.

Vous ne trouvez pas ce que vous recherchez ?

Contactez notre service client local si vous avez des questions ou si vous avez besoin de plus de détails ou d'une assistance technique.