Search FAQs
Video: Data Center Expert | How do I enable surveillance for NetBotz cameras?
Issue:
Enabling surveillance in StruxureWare Data Center Expert for NetBotz cameras.
Product Line
StruxureWare Data Center Expert (DCE)
InfraStruXure Central (ISXC)
NetBotz v3 Wall Appliance: 355/356 (NBWL0355/6) & 455/456 (NBWL0455/6)
NetBotz v3 Rack Appliance: 450/451 (NBRK0450/1), 550 (NBRK0550), & 570 (NBRK0570)
NetBotz Rack Monitor 750 (NBRK0750)
Environment:
StruxureWare DCE (any version)
NetBotz discovered by DCE (any supported version)
Cause:
This is for customers that require assistance in enabling surveillance for NetBotz cameras in DCE
Resolution:
Enabling surveillance in StruxureWare Data Center Expert for NetBotz cameras.
Product Line
StruxureWare Data Center Expert (DCE)
- Basic Appliance (AP9465)
- Standard Appliance (AP9470)
- Enterprise Appliance (AP9475)
- Virtual Appliance (AP94VMACT)
StruxureWare Central (SWC)- Standard Appliance (AP9470)
- Enterprise Appliance (AP9475)
- Virtual Appliance (AP94VMACT)
InfraStruXure Central (ISXC)
NetBotz v3 Wall Appliance: 355/356 (NBWL0355/6) & 455/456 (NBWL0455/6)
NetBotz v3 Rack Appliance: 450/451 (NBRK0450/1), 550 (NBRK0550), & 570 (NBRK0570)
NetBotz Rack Monitor 750 (NBRK0750)
Environment:
StruxureWare DCE (any version)
NetBotz discovered by DCE (any supported version)
Cause:
This is for customers that require assistance in enabling surveillance for NetBotz cameras in DCE
Resolution:
- Log into the Data Center Expert client.
- Ensure that the NetBotz Appliance with an integrated or attached camera pod is showing within Data Center Expert. If it has not been discovered yet, reference FA177081.
- Each NetBotz camera requires one Surveillance license. You can verify the licensing that you have installed by going to: System Menu > Server Administration Settings > License Keys. There will be a specific license type of Surveillance Pack with a total column and a used column.
- Select the Surveillance perspective.
- Right-click on one of the camera thumbnails and select Surveillance settings. TIP: You can select multiple thumbnails by holding down CTRL or SHIFT and selecting them.
- Mark the check box for License Camera.
- Enter the Data Center Expert IP address and configure the security options if necessary.
- Select the Post Mode that you would like to record the Surveillance clips for. There are other options to configure if deemed necessary.
- Select Apply and OK.
Released for:APC Canada
Explore more
Explore more