Browse FAQs



acdc1010 Hot Aisle Containment Rack Expansion Bundle Kit Installation (Manual)
... the PDU, UPS , or XR ... 3 . Know the ... the PDU, UPS , or XR ... ... the PDU, UPS , or XR ... ... the door frame assembly from the equipment ... ... panels onto each NetShelter VS (900 ... mm) or NetShelter VX (1070 ... ... a PDU or UPS , then a ... the PDU or UPS . ... When joining two NetShelter VX (1070 ... ... When joining two NetShelter VX (1070 ... ... doors of the UPS , PDU, ... ... When joining a NetShelter VS (900 ... ) to a NetShelter VX (1070 ... ... the door frame assembly to the equipment ...
Hardwiring to 120v, 208v, and 240v loads from a 208v/240v SmartUPS RT UPS
... addition to a selection of smaller 5kva plug in step-down transformers, APC manufactures 3 larger hardwire step-downs in 10kva and ...
In the NetShelter WX 6U Vertical cabinet, can the 2U UPS Mounting Bracket also be used on a 1U or 3U Smart-UPS?
Issue: It is unknown whether a 1U ot 3 U Smart- UPS can use the 2U mounting rail.
Are schematic drawings or 3D renderings available for NetShelter cabinets?
We do not offer STEP files or IGES files for any Smart- UPS .
Matrix-UPS frequently asked questions regarding installation, operation, and standards
... about the Matrix UPS ? Matrix UPS ... of a Matrix UPS . ... the APC Matrix UPS . ... . Matrix- UPS should be set ... ... to Matrix- UPS . ... , Matrix- UPS Input Select Tap ... 3 . Set Matrix- UPS EU (Electronics ... of Matrix- UPS IU (Isolation ... ... of Matrix- UPS or by its ... ... of Matrix- UPS IU to " ... ... , press all three buttons found directly ... ... current Matrix- UPS settings. ... to menu " UPS Tests" and ... Matrix- UPS Noises ... The Matrix- UPS will make certain ...
Video: How to Select the Correct Replacement Battery Cartridge (RBC) for your UPS
The UPS indicates battery replacement ... to when the UPS was first put into service . Smart- UPS and Back- ... ... maintenance for your UPS . UPS Replacement Battery Selector ... for your APC UPS and to see ... ... to know your UPS model #. ... To find your UPS model #, ... sticker on your UPS . ... bottom of your UPS . ... sticker indicates the UPS model number. ... row indicates the UPS serial number. ... year that the UPS was manufactured . ... is a unit manufactured in 2004. ... age of the UPS will also help ...
APC UPS Network Management Card (NMC) Compatibility Chart
... Which model of UPS Network Management Card ... supported in my UPS ? UPS Web/SNMP ... UPS Network Management Card ... UPS Network Management Card ... UPS Network Management Card 3 - ap9640, ... ... compatibility between current UPS models and discontinued ... ... use in other UPS systems can be ... UPS Model Single and Three Phase Smart- UPS with the following ... Matrix UPS with UPS firmware versions Y ... Three phase Symmetra models ... ... advantage of all UPS firmware enhancements. ... to monitor the UPS , and not ... ... NMC within the UPS must be used ... Single and Three Phase Smart- UPS with the following ...
Does the NetShelter CX interfere with a device's wifi signal? If it does, by what degree is the signal strength reduced?
Need to determine if the NetShelter CX can effect wifi signal strength. ... NetShelter CX ... Wireless devices can be installed inside a NetShelter CX cabinet. ... A wireless device was tested in the NetShelter CX manufacturing facility. The signal strength was affected by less than 10% in 3 of the test areas and by 38.46% in 1 of the areas. The
Can I install multiple APC SmartSlotAccessory Cards in one UPS?
... Cards in one UPS ? APC Branded UPS models with the ... ... Depending on the UPS type, it ... APC does manufacture a SmartSlot Expansion ... ... with any aforementioned UPS containing an existing ... The ap9600 attaches to the DB-9 serial port on your UPS system. You can daisychain multiple Expansion Chassis units off of one UPS . ... The ap9604blk contains three additional SmartSlots and is also considered a legacy product. When using all three slots or daisy-chaining the Triple Chassis, the 24VDC power adapter will be needed. ... Please see the following link for installing multiple SmartSlot accessories in a supported UPS system:
Why is my actual UPS runtime different from the quoted runtime on the APC web page?
... is my actual UPS runtime different from ... Smart- UPS ... is my actual UPS runtime different from ... ... a two or three discharge and charge ... ... that within a UPS that is not ... So providing the storage period and temperature has not exceeded the typical battery manufactures specification the battery will return to near full capacity, but sufficient recharge time, 48 - 72 hours must be allowed for the capacity to be recovered.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.