Browse FAQs



Universal Transfer Switch (UTS) – FAQ
Universal Transfer Switch (UTS) ... Universal Transfer Switch Product Line ... is the UTS’s transfer time while switching between Utility Power ... ... will engage its circuits and begin to ... ... as CPLD or Circuit Protection Load Disconnect ... ... unable to set Circuit 1 to UPS ... Circuit 1 is tasked ... Therefore Circuit 1 must be ... ... being an Automatic Transfer switch , however I ... APC UTS Generator Hardwiring ... APC UTS Automatic Remote ... ... should never be changed , unless the ... ... If the UTS circuit board were to ... Will my circuits have power?
What are the basic troubleshooting steps for the Universal Transfer Switch model UTS6H?
... steps for the Universal Transfer Switch model UTS6H? APC Universal Transfer Switch ... from the building circuit breaker panel. ... amperage of a circuit must be changed to accommodate the ... ... installed in the circuit , but the ... ... installed in the circuit , but the ... Use the Circuit Setup button to reset the affected circuit . Failure to reset the amperage for the affected circuit will cause nuisance circuit tripping, or ... ... Incorrect wiring to circuits . ... of the UTS circuits is not necessary ... However, Circuits 5 and 6 ... to the building circuit panel and must ...
What are the basic troubleshooting steps for the Universal Transfer Switch model uts10bi?
... steps for the Universal Transfer Switch model uts10bi? APC Universal Transfer Switch ... from the building circuit breaker panel. ... amperage of a circuit must be changed to accommodate the ... ... installed in the circuit , but the ... ... installed in the circuit , but the ... Use the Circuit Setup button to reset the affected circuit . Failure to reset the amperage for the affected circuit will cause nuisance circuit tripping, or ... ... Incorrect wiring to circuits . ... of the UTS circuits is not necessary ... However, Circuits 5 and 6 ... to the building circuit panel and must ...
What are the basic troubleshooting steps for the Universal Transfer Switch model UTS6 / UTS6BI?
... steps for the Universal Transfer Switch model UTS6 / ... APC Universal Transfer Switch ... from the building circuit breaker panel. ... amperage of a circuit must be changed to accommodate the ... ... installed in the circuit , but the ... ... installed in the circuit , but the ... Use the Circuit Setup button to reset the affected circuit . Failure to reset the amperage for the affected circuit will cause nuisance circuit tripping, or ... ... Incorrect wiring to circuits . ... of the UTS circuits is not necessary ... However, Circuits 5 and 6 ... to the building circuit panel and must ...
Replacement Fuses for the Universal Transfer Switch (UTS)
The following are examples of UL-listed, Branch Circuit Rated, Class CC fuses, that APC recommends. 15A:
Replacement Fuse types for the Universal Transfer Switch
The following are examples of UL-listed, Branch Circuit Rated, Class CC fuses, that APC recommends. 15A:
Legacy APC Refrigerant Charge
Legacy APC Refrigerant Charge ... Please note that the charge amounts below are "total" for the unit(s) Som units below have two independant circuits . ... CCT- 10 W/G ... 120 ozs ... TC- 10 W/G ... All charges are approximate, may vary +/- 5 lbs.
NetBotz 750 | Physical Description
2 Switched Outlet Provides power ... a maximum of 10 A. Activates ... ... for the door switch sensors (nbes0302 ... 6 Universal Sensor ports Used to connect APC by Schneider Electric ... 8 10 /100/1000 Network Port Provides a connection to the network. ... 9 Private LAN Provides a 10 /100/1000 connection to a private local area network and 48 VDC to an attached device. 10 Wireless Sensor Coordinator USB Port with Wireless NetBotz USB Coordinator (nbwc100u) installed. ... Relay Outputs can only be connected to Class 2 circuits . ... 17 Reset Switch Reboots the appliance.
ACRP1XX, ACRD5XX, ACRP5XX, and ACRC5XX Parts List
... part numbers can change . ... some may have changed . ... CONTACTORs, & CIRCUIT BREAKERs ... CONTACTORs, & CIRCUIT BREAKERs ... 1 200- 240v 0w3121 CABLE ASSY ... ... ATS 200- 240v #2 0w3125 ... ... Connection Kit acac20012 Circuit Board For Compact ... Circuit Board For Compact ... Circuit Breaker 2P 5A 240v ... 272 417 r0357 Circuit Breaker 2P ... ... 272 317 r0357 Circuit Breaker 3P ... ... 273 417 r0457 Circuit Breaker 3P ... ... 273 317 r0427 Circuit Breaker 3P ... ... 273 317 r0457 Circuit Breaker 3P 20a 240v ... 273 417 r0487 Circuit Breaker 3P 30a 240v


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.