Technical FAQs

Ask a Question

How to set up an IP Address for an ACRC100 unit through the Display

Issue: 
How to set up an IP Address for an ACRC100 unit through the Display.
 
Product line: 
ACRC100.
 
Environment: 
All Serial Numbers.
 
Cause:
Install, Set-Up.
 
Resolution:
 
To set up the network configuration for an ACRC100 unit through the display.
 
  1. Press the <ESC> key until you get to the Main Menu On/Standby screen.
  2. Press the <DOWN> arrow until you get to the heading configure network.
  3. Press <ENTER> and you will be prompted for a password
  4. To enter password use the arrows to select the character and then press <ENTER> to move to the next character.
  5. Default Password:  <apc>
  6. After the last character is selected press <ENTER>
  7. Press the <ENTER> key to move the cursor to the number you need to change.
  8. To change heading place arrow at the beginning of the heading and the use the up or down arrow.
  9. Press <ESC> until you get back to the main menu.
 
Was this helpful?
What can we do to improve the information ?