Browse FAQs



LDAP/LDAPS Configuration with KVM1116P, KVM2116P, and KVM2132P Digital IP KVM Switches
Need assistance or instructions on configuring LDAP/LDAPS with Digital IP KVM Switches ... KVMXXXX Digital IP KVM Switches ... 3. Follow the Installation Wizard to complete the procedure. ... 5 . Under Available Standalone Snap-ins, double click Active Directory Schema. ... 5 . Fill in the dialog box to match the entries for Description and Common Name shown below, then click OK to complete the procedure. ... 5 . On the Attributes page, click Add. ... CN=Users node . ... 5 . On the Attribute Editor page of the dialog box, select iKVM-userprofile from the list.
Data Center Expert | What virtualization environments are supported?
... the Data Center Expert virtual appliance? ... StruxureWare Data Center Expert (DCE) ... StruxureWare Data Center Expert (all verisons ... ... found within the EcoStruxure IT Help Center ... ... -Center- Expert -Virtual- ... ... The Data Center Expert v7. ... The full-featured demo of the virtual appliance monitors up to five device nodes and one surveillance node . You can purchase a license key to upgrade to a production version to monitor additional device nodes and activate supported applications, or to migrate from a server hardware version to a virtual appliance.
APC Switched Rack PDUs - any pending outlet commands are lost when PDU Network Management Interface is rebooted
... for more than 10 minutes ... be any valid node's IP on the ... ... take 3- 5 seconds each depending ... Do not power the Rack PDU's network connection by the same Rack PDU's outlets (and turn it off for longer than 10 minutes) - ... - Since the watchdog timer expires in about 9.5- 10 minutes, make sure the outlet on/off/reboot time for the specific outlet powering the Rack PDU's network connection is not off for more than 9 minutes.
Creating an Aggregate Device within the KVM Access Software
... ships with KVMXXXX Digital IP KVMs) ... wishing to consolidate nodes within their KVM ... ... as a single node , and only ... ... I have 300 node license but have ... ... purchase a 900 node license to cover ... effectively creating 150 nodes in total. ... ... the amount of nodes I need to ... 5 .) Optional ... ... , Dell DRAC 5 , Dell iDRAC ... ... , Dell DRAC 5 , Dell iDRAC ... 5 .) When ... Additional Notes and FYIs: ... blades = 17 nodes ... then the total nodes of KVM Port ... All connection to KVM Access in the Aggregate Only section count as one node . The following rules need to be taken into account:
NetBotz 455 | Physical Description
3 A-Link port Used for cascading NetBotz sensor pods and temperature and humidity sensors with digital displays. Provides communications and power to the connected devices over standard CAT- 5 cabling with straight-through wiring. 4 10 /100 Base-T network port Provides for a 10 /100 Base-T network connection and power through Power-over-Ethernet (PoE).
NetBotz 250 | Physical Description
5 Beacon Port Used for connecting an alarm beacon (AP9324). ... 9 10 /100 Network Port Provides the connection to the network. ... 10 A-Link Ports Used to cascade NetBotz Rack Sensor Pod 150s (nbpd0150), or connect Temperature/Humidity Sensors with Digital Display (ap9520th). Provides communications and power using standard CAT- 5 cabling with straight-through wiring.
NetBotz 750 | Physical Description
NetBotz version 5 NetBotz v 5 .X ... a maximum of 10 A. Activates ... ... humidity sensors with digital displays) over standard CAT- 5 cabling with straight ... 5 Rack Access Ports ... ... party 0- 5 V sensors. ... , 0- 5 V sensors require ... NetBotz 0- 5 V sensor cable ... 8 10 /100/1000 Network Port Provides a connection to the network. ... 9 Private LAN Provides a 10 /100/1000 connection to a private local area network and 48 VDC to an attached device. 10 Wireless Sensor Coordinator USB Port with Wireless NetBotz USB Coordinator (nbwc100u) installed.
NetBotz 450/550/570 | Physical Description
10 Sensor ports ( ... party 0- 5 V sensors. Standard third-party 0- 5 V sensors require the NetBotz 0- 5 V Sensor Cable (nbes0305). nbrk0450/550 - 5 /24 VDC 950ma). nbrk0570 - 5 /24 VDC (200ma). ... 13 A-Link port Used for cascading NetBotz sensor pods and temperature and humidity sensors with digital displays. Provides communications and power to the connected devices over standard CAT- 5 cabling with straight-through wiring.
APC Environmental Sensors FAQ
The APC dedicated sensors use standard RJ45 connectors and may be extended with standard CAT- 5 ethernet cables and either RJ45 double female couplers or a patch panel. ... What are the benefits of the LCD digital sensor ap9520th? ... (4) Total of 10 T/H measurement points, vs. the two basic local probes.
Data Center Expert | Trial version VM appears to have 25 nodes available.
... Machine or VM version shows this same 25 node license key in the user interface however until activated, will only allow 5 nodes to ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.