How can I mass configure a Network Management Card (NMC) or NMC embedded product?
How can I mass configure a Network Management Card (NMC) or NMC embedded product? ... How can I mass configure or configure ... ... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but ... ... AP9312TH, MasterSwitch 1 /2) ... ... Management Card, mass configuration of those ... ... and uploading a single configuration file ( ... More information on this topic ... ... file from a single Network Management Card ... ... firmware versions, one option is to ... ... file to a single Network Management Card ... Method 1 - via Web ... Method 1 - ISX Manager ... ... Manager offers a mass configuration utility. ... ISX Manager for information on performing the mass configuration. The mass configuration option in ...