Browse FAQs



Data Center Expert | How do hardware and software support contracts work?
... work for StruxureWare Data Center Expert . StruxureWare Data Center Expert (DCE) StruxureWare Data Center Expert (all versions ... StruxureWare Data Center Expert appliances come with ... The Data Center Expert appliance and any ... ... a default 25 nodes (covered under ... as each additional node license . Modbus license keys and surveillance keys do not currently ... StruxureWare Data Center Expert Appliances can have ... ... virtual machine activation key (AP94VMACT) ... ... your server and license keys back under support ... ... amount of Device Nodes Installed ... number of install licenses .
Data Center Expert | Trial version VM appears to have 25 nodes available.
... Machine or VM version shows this same 25 node license key in the user interface however until activated, will only allow 5 nodes to ...
Data Center Expert | What virtualization environments are supported?
You can purchase a license key to upgrade to a production version to monitor additional device nodes and activate supported applications, or to migrate ...
Data Center Expert | Migrating from a Physical Appliance to a Virtual Appliance
StruxureWare Data Center Expert (DCE) StruxureWare Data Center Expert (all versions ... As the data center is moving away ... ... the AP94VMACT activation key to activate the ... ... server already has licensing on it ( ... base 25 device nodes and 1 surveillance node ) your will ... License keys are tied to ... ... contracts for the license keys and the server ... can reset the license key passcodes so that ... used again to license the virtual server ... ... new servers/ licenses . ... support for the license keys against this mac ... ... redeem the activation key passcode as well ...
Data Center Expert | Why does StruxureWare not accept my One Time passcode?
StruxureWare Data Center Expert is not accepting ... StruxureWare Data Center Expert (DCE) ... StruxureWare Data Center Expert (all versions ... SturuxureWare Data Center Expert requires a 64 character license key that is created ... passcode and the Data Center Expert's MAC address. StruxureWare Data Center Expert (DCE) ... ... to gather specific information about the alert ... ... when purchasing a license key is not the actual license . ... passcode to a license key . ... AP9465 = StruxureWare Data Center Expert Basic ... ap9470 = StruxureWare Data Center Expert Standard ... AP9475 = StruxureWare Data Center Expert Enterprise
Data Center Expert | Getting Started
... started with a Data Center Expert Appliance. StruxureWare Data Center Expert (DCE) StruxureWare Data Center Expert (all versions ... ... Deploying the Physical Data Center Expert Appliance ... Deploying the Virtual Data Center Expert Appliance ... restricted to 5 nodes . ... you have purchased licensing , continue to ... the passcodes for licenses . ... deploy the StruxureWare Data Center Expert Virtual Appliance? ... of storage that Data Center Expert has within VMWare ... Getting Data Center Expert on the Network ... ensuring that your Data Center Expert (DCE) ... ... Settings for StruxureWare Data Center Expert
Can I transfer license keys between StruxureWare Data Center Expert servers?
Product Line: StruxureWare Data Center Expert (DCE)
Video: Data Center Expert | How do I enable surveillance for NetBotz cameras?
You can verify the licensing that you have installed by going to: System Menu > Server Administration Settings > License Keys .
IPMI Overview
A separate processor called a Baseboard Mgmt Controller (BMC) runs along side the core/main processor in a system to allow monitoring of the system’s status, environmental info , etc internally, regardless of the health of the core processor. ... IPMI is supported on the NetBotz 500 , 420, 320 with a valid Premium Software Module key installed IPMI is supported on the NetBotz 450, 455, 550, and 570 units with a 5 node monitoring pack (nbwn0006) installed.
Creating an Aggregate Device within the KVM Access Software
... wishing to consolidate nodes within their KVM ... ... as a single node , and only requires a single license . ... I have 300 node license but have 300 ... ... purchase a 900 node license to cover all ... effectively creating 150 nodes in total. ... ... the amount of nodes I need to ... IP Key in the Aggregate ... Port Key in the access ... ... Username/Password Key in a username ... ... /password field Key in the information so that the ... name and password information under certain single ... ... Provide any additional information in the Contact ... ... according to the information in the table ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.