Browse FAQs



DAC, Cancoil Installation Manual
... how to properly install a legacy DAC ... Install Air Cooled Condenser Installation and Operating Instructions DAC Air Cooled Condensers For information ... Cancoil air-cooled condensers have been ... ... equipment, proper installation and set- ... ... be used if air-cooled quipment is located ... Installation Date __ ... ... properly sized and installed to insure oil ... ... risers should be installed with a trap ... Cancoil air-cooled condensers are available ... variety of optional fan cycling controls, ... are shipped without fan controls. Check ... ... amperage on the fan motor(s ... ... . Verify the fan rotation direction.
Where can I get support for APC and MGE Products?
Air Cooled Chillers ... Installation Services ... Outdoor Enclosures ... Software Installation
APC Schneider Cooling Unit Identification
... Expansion A= Air Cooled E= Air Cooled ... Main A= Air Cooled ... ) A= Air Cooled ... ) A= Air Cooled ... ) A= Air Cooled E= Air Cooled w/Multicool R= Air Cooled w/Remote ... ... -5T Air Cooled or ... 0 A= Air Cooled SC= Air Cooled Self-Contained IR= Air Cooled Indoor Condenser IG= Air Cooled Indoor Condensing OR= Air Cooled Outdoor Condenser OG= Air Cooled Remote Indoor Condensing ... ) A= Air Cooled E= Fan Coil/Evap ...
Refrigerant charging table for a Uniflair Unit
Install . ... Air-cooled DX units must be connected to a remote outdoor condenser. Systems with remote outdoor condensers must have discharge and liquid lines from the equipment to the condenser. ... Install all refrigerant lines in accordance with applicable industry guidelines as well as local and national codes and regulations. ... • All refrigerant pipes are installed with proper supports and approved refrigerant line clamps. ... When brazing field- installed copper refrigeration lines, use a nitrogen purge to minimize ... Install a ball valve before the micron gauge to prevent damage to the micron gauge during charging.
What are the operational conditions for an InRoom (Stulz) Unit
Install ... Outdoor ambient conditions: Lower limit: -10°C (14°F) Upper limit: Depending on selected condenser ... Maximum equivalent length of piping between the cooling unit and the air cooled condenser: 60 m (200 ft)
How to clean Heatcraft-Larkin Refrigeration condensers
Install , Repair ... Air cooled condensing units require a minimum of maintenance. ... All of the condenser fan motors have sealed ball bearings. ... Reference Heatcraft-Larkin Refrigeration Products Remote Air Cooled Condensers Manual. Bulletin H-IM-73A June 2000 Part Number 90800801
Why does only one fan spin on my APC step down transformer (part numbers AP9626/27/28, SYTF2, SRT5KTF, SRT5KRMTF)?
APC step down transformers come with two fans installed . One is the primary AC fan that is used for forced air cooling of the transformer.
Fan Power Supply on a ACRC1XX
Issue: This document contains the correct procedure on how to Remove or Install a Fan Power Supply on a ACRC1XX .
What is the cfm rating of the NetShelter CX with ar4703 installed?
Issue: Customers want to know the cfm rating of NetShelter CX cabinets with the ar4703 fan booster installed .
LNE Receiver Installation
Condenser receiver, LNH, aircooled , Installation manual, mounting


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.