Browse FAQs

Does the NTP need to be configured on the Galaxy VS internal NMC and the optional AP9644 NMC for all parallel or single Galaxy VS?

Published date: 09 March 2020

Issue:
Does the NTP need to be configured on the Galaxy VS internal NMC and the optional AP9644 NMC for all parallel or single Galaxy VS


Product line:
Galaxy VS


Environment:
Galaxy VS


Cause:
Configuring NTP on both Galaxy VS internal NMC and the optional AP9644 NMC can cause issues like excessive time stamp events in the log files.  The Galaxy VS internal NMC and the optional AP9644 NMC communicate between each other and they will try sync the date and time which can cause a loop of trying to set the date and time.


Resolution:
Ensure that only one network management interface in the entire UPS system (single or parallel) is set to synchronize time.
 

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.