Are the NetShelter VX Seismic cabinets and 2-Post Racks OSHPD compliant?
Published date:
22 November 2019
Issue:
the question has been risen if a NetShelter VX Seismic cabinet is OSHPD compliant.
Product Line:
NetShelter VX Seismic, 2-Post Rack
Environment:
AR2144BLK, AR2145BLK, AR201: all serial ranges.
Cause:
The only seismic documents on the product pages of AR2144BLK and AR2145BLK are the NEBS GR-63-CORE Zone 4.
There are no seismic documents on the product page of AR201.
Resolution:
Several Smart-UPS were tested and approved for installation with NetShelter VX Seismic and AR201 during OSHPD Special Seismic Preapproval (OSP) testing. Please see the attachment.