Does the ACSC automatically restart after a high head pressure alarm?
Published date:
11 June 2020
Issue:
Does the ACSC automatically restart after a high head pressure alarm?
Product line:
ACSC100, ACSC101
Environment:
InRow Cooling Cause:
Resolution:
Yes, if the ACSC sees the HP switch open, it will switch into idle mode and then attempt to restart after a 2 minute delay. If the unit had the HP switch open three times within 30 minutes, the ACSC will go into Persistent High Discharge alarm and will lock out the compressor. This alarm will need to be reset manually.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.