Can the NetShelter CX be deployed in any room or space?
Published date:
21 February 2020
Issue:
Where can the NetShelter CX be deployed?
Product Line:
NetShelter CX
Environment:
All versions and serial ranges.
Cause:
It's wise make sure that the NetShelter CX is suited for the environment in which it's to be installed.
Resolution:
Optimal performance of these cabinets requires suitably ventilated space or building HVAC system.
The NetShelter CX is not suitable for installation in a small unventilated space.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.