Технические часто задаваемые вопросы

Does the NTP need to be configured on the Galaxy VS internal NMC and the optional AP9644 NMC for all parallel or single Galaxy VS?

Дата публикации: 09 March 2020

Issue:
Does the NTP need to be configured on the Galaxy VS internal NMC and the optional AP9644 NMC for all parallel or single Galaxy VS


Product line:
Galaxy VS


Environment:
Galaxy VS


Cause:
Configuring NTP on both Galaxy VS internal NMC and the optional AP9644 NMC can cause issues like excessive time stamp events in the log files.  The Galaxy VS internal NMC and the optional AP9644 NMC communicate between each other and they will try sync the date and time which can cause a loop of trying to set the date and time.


Resolution:
Ensure that only one network management interface in the entire UPS system (single or parallel) is set to synchronize time.
 

 

Вы нашли ответ на свой вопрос?

Как мы можем улучшить информацию?

Не нашли то, что искали?

Обратитесь к нашей команде по обслуживанию клиентов для получения информации о технической поддержке, помощи в составлении претензий и другого.