Технические часто задаваемые вопросы

How many 0U accessory channels (RCC's) are included with NetShelter SX cabinets, and how manu PDUs can fit into them?

Дата публикации: 12 June 2019

Issue:
Customers need to know how many 0U accessory channels are in each cabinet, and how many PDUs can mount into them.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
Customers need to plan installation of PDUs and cable management.

Resolution:
 

  • All 1070 mm deep NetShelter SX cabinets have 2 0U accessory channels.
  • All 1200 mm deep NetShelter SX cabinets have 4 0U accessory channels except the Networking cabinets.
  • All 1200 mm deep NetShelter SX Networking cabinets (AR3340 and AR3347) have 2 0U accessory channels.
Each 0U accessory channel can accommodate two (2) full height PDUs.
  • A 1070 mm deep cabinet can mount up to 4 full height 0U PDUs.
  • A 1200 mm deep cabinet (except AR3340 and AR3347) can mount up to 8 full height 0U PDUs.
  • All NetShelter SX and SX Networking cabinets offer 0U accessory channels as a 

Вы нашли ответ на свой вопрос?

Как мы можем улучшить информацию?

Не нашли то, что искали?

Обратитесь к нашей команде по обслуживанию клиентов для получения информации о технической поддержке, помощи в составлении претензий и другого.