Технические часто задаваемые вопросы



Can I use a serial connection for shutdown when I have a Network Management Card installed in my SU, SUA, SURT, or SUM series Smart-UPS?
... using a Network Management Card may result ... ... Smart-UPS installations that include a Network Management Card, but ... ... using a Network Management Card with your ... Network Shutdown to manage device shutdowns for ... ... using a Network Management Card, it ... ... UPS is on battery , when it ... has reached low battery . ... via the Network Management Card web interface ... To shutdown a device via simple signaling serial communications while also using a Network Management Card: ... 1 ) Use the optional 2) Ensure that "Basic Signaling Shutdown" is enabled in the Network Management Card interface
BMS AP9921X-AP9922; what specific alarms will set the “Management Controller Alarm?
... set the “ Management Controller Alarm? ... Battery Management System (BMS ... ... set the “ Management Controller Alarm? ... ... alarms listed below activate the Management Controller LED. ... have at least one current sensor, one ambient temperature sensor, and one pilot battery temperature sensor to ... Reset the Battery Management System using the ... ... lead-acid batteries only): The batteries are reporting low ... ... : When the Battery Management System detects this ... damage to the batteries . One or more units ... ... type) were included in the hardware ... ... is done, one must insure that ...
Why am I receiving a "serial communication lost" message from my Network Management Card?
... from my Network Management Card or Web ... ... /SNMP Card include (but are ... Environmental Monitoring Unit 1 (AP9312TH) UPS Network Management Card 1 (NMC1) ... ... beginning with v 1 .X, ... ... ID and Last Battery Replacement Date are ... Web/SNMP Management Card or Network Management Card installed . ... a card is installed in a Symmetra ... Shutdown Low Battery ... Assuming your Network Management Card firmware is ... ... the last " battery replacement date" ... Web/SNMP Management Card (ap9606) or Network Management Card (AP9617 ...
UPDATED MARCH-2016: Unable to access my APC Network Management Card (NMC) enabled device via HTTPS (SSL/TLS)
... their APC Network Management Card (NMC ... ... has their Network Management Card product configured ... One such vulnerability is ... ... v34.0 installed . ... v11.0 installed . ... An AP9631 Network Management Card is configured ... ... has Chrome v39 installed . ... error messages may include : Network Management Card 1 (NMC1) ... ... an embedded Network Management Card 1 include (but are ... ), AP9921X Battery Management System, ACFXXX ... Network Management Card 2 ( ... ... an embedded Network Management Card 2 include (but are ... ... who uses any one of the products ... One such example is ...
How do I properly install/uninstall my SmartSlot accessory card into my UPS?
... do I properly install /uninstall my ... ... UPS Models - Single and Three Phase including Smart-UPS ... Device UPS Management accessories including but not limited ... UPS Network Management Card 1 and 2 Interface Expander 1 /2 ... /JBUS Building Management Card All installation /uninstallation scenarios ... ... The procedure for installing /removing a ... ... of ap9630 Network Management Card 2 ... of ap9630 Network Management Card 2 ... can remove and install the SmartSlot card ... ... to remove/ install an accessory depending ... ... the DC ( battery ) power. ... to remove or install a SmartSlot accessory ...
Why are the battery charge LEDs flashing on a Smart-UPS?
Battery Charge LED Bar ... ... than the low battery signal warning time ... ... than the low battery signal time, the battery charge graph LEDs ... Option 1 : ... Reset the low battery signal time to ... ... with the low battery signal warning time ... ... , then the battery bar graph LEDs ... ... setting the low battery signal warning time ... ... , the low battery signal time is ... UPS battery ... or replace the battery . ... , yet the batteries are consumable items ... As the batteries age, they ...
Symmetra LX Battery Module Information Missing within v6.X.X Network Management Card Firmware Web Interface
... this specific issue, this relates specifically to the last battery installed within a Symmetra LX system, including any batteries located in any Extended ...
Batteries discharged to a low voltage in a single phase Symmetra frame
... need a fresh battery (greater than ... inserting this fresh battery module, it ... remove all discharged battery modules installed in the system (this includes any battery modules in connected ...
Video: Troubleshooting no communication between UPS and PowerChute Business Edition
Troubleshooting Windows Serial Communications ... PowerChute Business Edition Installation Guide
BMS AP9921X-AP9922 Battery Management System; high battery voltages on 40 Jar battery applications
... AP9921X-AP9922 Battery Management System (BMS) installed on a 40 Jar battery solution; such ... on MGE UPS battery systems, it’s ... high voltages on one or more B side batteries .


Результаты 1 - 10 of 99

Не нашли то, что искали?

Обратитесь к нашей команде по обслуживанию клиентов для получения информации о технической поддержке, помощи в составлении претензий и другого.