Технические часто задаваемые вопросы



Why does my H-Type Power Conditioner make a high pitched noise?
APC H Type Power Conditioner, Line-R Automatic Voltage Regulator, buzzing, humming, h10blk, H15BLK, s10blk, S15BLK, ...
What is AVR (Automatic Voltage Regulation)?
Product Line: Line-R , Back-UPS, Back-UPS PRO, Smart-UPS and APC AV.
What does APC have available for Line Conditioning?
Product Line: Line-R , APC AV H-Type
What are the differences between the Back-UPS RS and the Back-UPS XS models (Does not Include BX/BR LCD Models)
... Back-UPS RS and the Back ... Product Line : ... /XS/ RS ... Back-UPS RS and the Back ... ... Back-UPS RS models have both 1- line 2-wire ... modem data- line protection and 10 ... has 1- line 2-wire ... 2. The Back-UPS RS models have both Boost* and Trim** as features of Automatic Voltage Regulation (AVR), where as the Back-UPS XS only has Boost.
How to Install a OROA or A LAC Valve as part of a Flooded Receiver Package
C= Line from the bottom header of the condenser. R = Line from the valve to the Flooded Receiver.
What are the basic troubleshooting steps for the Back-UPS RS model br1000g?
What are the basic troubleshooting steps for the Back-UPS RS model br1000g? Product Line : APC Back-UPS RS ... The unit is performing an automatic self test.
What are the basic troubleshooting steps for the Back-UPS RS model br700g?
What are the basic troubleshooting steps for the Back-UPS RS model br700g? Product Line : APC Back-UPS RS , ... The unit is performing an automatic self test.
What are the basic troubleshooting steps for the Back-UPS RS model br1300g / br1500g?
What are the basic troubleshooting steps for the Back-UPS RS model br1300g / br1500g? Product Line : APC Back-UPS RS , ... The unit is performing an automatic self test.
APC Schneider Cooling Unit Identification
Product line : MA= 600 /3/ ... R =Upflow MA= 600 /3/ ... EA= 600 /208/ ... R = Upflow MA= 600 /3/ ... EA= 600 /208/ ... MA= 600 /3/ ... EA= 600 /208/ ... MA= 600 /3/ ... MA= 600 /3/ ... R = Upflow 6= 600 /3/ ... R = Air Cooled ... R = Remote Condensing R = Remote X ... R = Remote X ... MA= 600 /3/ ... MA= 600 /3/ ...


Результаты 1 - 10 of 88

Не нашли то, что искали?

Обратитесь к нашей команде по обслуживанию клиентов для получения информации о технической поддержке, помощи в составлении претензий и другого.