Browse FAQs

Symmetra MW; when I press the “Test Email” button the display doesn’t send test email

Published date: 07 March 2016


 
Issue:
Symmetra MW; when I press the “Test Email” button the display doesn’t send test email
 
 
Product line:
Symmetra MW
 
 
Environment:
All models/ all serial numbers
 
 
Cause:
When I press the “Test Email” button the display doesn’t send test email.
 
 
Resolution:
First confirm that all Display Network and Email configuration settings are configured properly.
Test if you can ping the display and also test you can ping the DNS service and backup DNS server, if you can then try to reboot the display to save the changes made to the email settings.
 
To reboot the display locate the calibration/ reboot display feature under the service settings screen or use the pin hole reset button top of the display. Please note that rebooting the display will not affect the UPS operation mode, it is safe to do while load is on the UPS.
 
Display reboot should allow the emails settings to save and now the “Test Email” functionality should work.
 
 


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.