Browse FAQs



Unlicensing a Camera from NetBotz Central Results in Deletion of Associated Surveillance Pictures
Note that only unlicensing cameras can free up Surveillance license nodes .
Data Center Expert | Migrating from a Physical Appliance to a Virtual Appliance
... located within knowledge base . Note that ... (beyond the base 25 device nodes and 1 surveillance node ) your will need to log into ...
Data Center Expert | Discovering a NetBotz 700 Series Appliance
FA297815 Instructions for enabling surveillance for NetBotz cameras in Data Center Expert can be found in knowledge base .
Data Center Expert | What Cameras are supported?
Future revisions of the NetBotz 750 and 755 may ... motion detection feature so surveillance based on motion will not be available on those cameras.
Video: How do I retrieve surveillance clips in StruxureWare Data Center Expert
Retrieving surveillance clips in StruxureWare ... NetBotz NetBotz discovered by DCE and licensed for surveillance ... assistance in retrieving NetBotz camera clips in ... 1) Open the DCE Client and go to the Surveillance perspective. ... 3) Within the Thumbnails pane, you will see the camera thumbnails for your NetBotz Appliances that are in the group you selected. ... If a thumbnail shows a red circle with a cross-line through it, the camera has not been licensed for surveillance . See knowledge base for instructions. ... Clips are stored according to the NetBotz Appliance date/time, not the DCE Appliance date/time.
NetBotz 700 Series | Motion alerts in DCE do not contain camera images
NetBotz 750/755 ... NetBotz 700 Series - NetBotz Wall Monitor 755 ... - NetBotz Rack Monitor 750 ... NetBotz 750 / 755 ... ... .7 and NetBotz "Botzware" ... 5.2 surveillance is enabled. ... up in the surveillance view. ... also configured for surveillance at the same ... ... the way previous NetBotz alerts would contain ... Please note that the NetBotz 165 camera pod must be enabled for surveillance to show these images. Please also note that the images will in no way be directly linked to the alert, you will need to search for the images based on the timeframe of the known alert.
Power Specifications for NetBotz 500
Power Specifications for NetBotz 500 ... NetBotz ... NetBotz version 2 500 ... Power Specifications for NetBotz 500 ... -Power Supply Inefficiency: 15 Watts ... -Wallbotz 500 Power Consumption - Minimum Configuration ( Base Unit + 1 docked Camera Pod + 1 docked Sensor Pod)
NetBotz TFTP upgrade/recovery procedure
NetBotz TFTP upgrade procedure ... NetBotz version 3 NetBotz model: 355 ... Optional NetBotz firmware upgrade/ ... ... for restoring a NetBotz appliance to default ... behavior on a NetBotz appliance. ... segment as the NetBotz Appliance. ... plugged into the NetBotz Appliance during this ... ... com for your NetBotz Appliance (355 ... ... ) Set the base directory of your ... ... traffic between the NetBotz Appliance and the ... ... refer to knowledge base . ... power from the NetBotz Appliance while keeping ... ... be at a NetBotz > prompt. ... address for the NetBotz Appliance) ... address for the NetBotz Appliance) ... mask for the NetBotz Appliance)
NetBotz | Wireless Network Basics
NetBotz Rack Monitor 700 ... - NetBotz Rack Monitor 750 ... - NetBotz Wall Monitor 755 ... NetBotz 400-500 ... - NetBotz Rack Monitor 570 ... - NetBotz Rack Monitor 450 ... - NetBotz Wall Monitor 455 ... NetBotz Rack Monitor 200 ... - NetBotz Rack Monitor 250 ... NetBotz Rack Monitor 250 ... NetBotz Wireless Sensors ... of a host NetBotz appliance, a ... ... (700 series NetBotz Appliance) collects ... and generates alerts based on sensor readings ... ... port on the NetBotz Appliance. ... connected to the NetBotz appliance. ... a range of 15 m (50 ... ... port on the NetBotz appliance.
NetBotz 700 Series | Wireless Network (Coordinator / Sensors)
NetBotz Rack Monitor 700 ... - NetBotz Rack Monitor 750 ... NetBotz Rack Monitor 700 ... NetBotz Wireless Sensors ... of a host NetBotz appliance, a ... ... (700 series NetBotz Appliance) collects ... and generates alerts based on sensor readings ... ... port on the NetBotz Appliance. ... connected to the NetBotz appliance. In a data center environment where obstructions are common, a range of 15 m (50 ft) is typical. ... Connect one nbwc100u (USB Coordinator & Router) to a USB Type A port on the NetBotz appliance. Power the routers: Connect each router to an AC-USB adapter, not the NetBotz appliance.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.