Technical FAQs

Ask a Question

Where can I find Hazardous Materials Quantities for C&D Technologies batteries used in MGE EPS, Galaxy and galaxy PW products?

 

Issue:
New building code requires Hazardous Materials Quantities, here we have C&D Technologies battery information


Product line:
EPS 6000, EPS 7000, EPS 8000, Galaxy PW, Galaxy 5000, Galaxy 4000


Environment:
All VLRA batteries


Cause:
Building Code  requirement


Resolution:
Attach is C&D Technologies battery information of  Hazardous Materials Quantities

An example:
G5K 40KVA  with one string of UPS12-490FR will have 36 batteries, 100% run time 61 min.
 Each battery has 6 Cell  so 36 battery have total  216 cells attached information show 0.3 Electrolyte Volume per Cell  (Gal)  so 216 X 0.3 =  64.8 Gal of Electrolyte




 
 
Was this helpful?
What can we do to improve the information ?