Technical FAQs

Ask a Question

What is the center-to-center dimension of the square holes on the NetShelter VX Seismic side brace?

Issue:
The manual does not state the dimensions of the holes on the side braces that are used to set the mounting rail depth. 

Product Line:
NetShelter XV Seismic

Environment:
All versions and serial ranges.

Cause:
The hole to hole dimension is needed check horizontal mobility of the mounting rails in the cabinet. 

Resolution:

The dimension of the square holes in the side brace is 31.75mm center to center. 
The holes are 9.5mm square. 
 
Was this helpful?
What can we do to improve the information ?