Technical FAQs

Ask a Question

802.3 Network Compliance with Netbotz Version 1 Appliances

Issue:

802.3 Network Compliance with Netbotz Version 1 Appliances

Product Line:
NetBotz

Environment:

NetBotz version 1

Cause:

Article Title: 802.3 Compliance for NIC Interface for NetBotz Version 1 Appliances

The following is a compliance letter for the 802.3 network interface on the NetBotz Version 1 Appliances.

Resolution:


NetBotz part number 02236 Rev 00 Letter of Compliance For WallBotz 310C/400C, RackBotz 310C/400C (NetBotz product numbers: NBWL0310C, NBWL0400C,NBRK0310C, NBRK0400C)

For the products listed above, NetBotz claims the following:

NetBotz uses Agere part LU3X31FT (Single-Port 3V 10/100 Ethernet Transceiver TX/FX). Agere’s datasheet for the LU3X31FT states that it “was designed from the beginning to conform fully with all pertinent specifications, from the ISO*/IEC 11801 and EIA/TIA 568 cabling guidelines to ANSI X3.263 TP-PMD to IEEE 802.3 Ethernet specifications” and has “IEEE 802.3u Clause 28 compliant auto-negotiation for full 10M and 100M control” and also has an “IEEE 802.3 compatible 10Base-T and 100Base-T physical layer interface and ANSI X3.263 TP-PMD compatible transceiver.”
NetBotz followed Agere’s design and implementation recommendations with respect to the LU3X31FT
ISO is a registered trademark of The International Organization for Standardization. EIA is a registered trademark of The Electronic Industries Association. ANSI is a registered trademark of The American National Standards Institute, Inc. IEEE is a registered trademark of The Institute of Electrical and Electronics Engineers, Inc.
 
Was this helpful?
What can we do to improve the information ?